Hello community,
I have one question about usage of redundant boot and secondary boot image.
Following boot mode are supported redundant boot and it can boot from secondary image.
And others not support redundant boot
Is it correct?
Best regards,
Ishii.
解決済! 解決策の投稿を見る。
Hello, Ishii!
Appears, You are right: in case of NAND ECC errors, secondary boot option is also provided.
I agree with Your considerations above.
Regards,
Yuri.
Hello,
The redundant boot is supported for MMC/eMMC and SD/eSD compliant devices.
Have a great day,
Yuri.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
Hello Yuri,
Thank you for your quick response.
And sorry for my bad question.
I hope to know when is secondary image used by boot ROM.
I think it has 4 pattern
In case 3, If it is correct, it seems that all internal boot mode will be used secondary image if authenticate is failed.
Which boot mode does it support to use secondary image in this case?
If other case it is used secondary image, please let me know.
Best regards,
Ishii.
Hello, Ishii !
The secondary image is used in the Closed mode, if Authenticate failed.
No more scenarios for the redundant mode.
    For the Closed mode, if there are failures during primary image authentication, the boot
ROM turns on the PERSIST_SECONDARY_BOOT bit (see Table 8-6) and performs the
software reset. (After the software reset, the secondary image is used.)
Regards,
Yuri.
Hello Yuri,
Thank you for your answer.
I understand that the secondary image is used in the closed mode only.
If I use Parallel NOR-Flash boot with closed mode, where is a location of Secondary Image Table?
Boot Rom will read table from address 0x200 is correct?
IVT offset is different both NOR and OneNAND in table 8-23.
But I can't find location of secondary image table for NOR flash boot
both Reference Manual and Security Reference Manual.
Best regards,
Ishii.
Hello,
The redundant boot is supported only for MMC/eMMC and SD/eSD.
Regards,
Yuri.
Hello Yuri,
I confused now.
Boot ROM are set secondary image persistent bit only following 2 condition.
So, the secondary image may only be referenced during a NAND boot or
redundant boot (it support for MMC/eMMC/SD).
Other boot mode(Parallel NOR, OneNAND, EEPROM) have no time to referenced secondary imae.
Is it correct?
Best regards,
Ishii.
Hello, Ishii!
Appears, You are right: in case of NAND ECC errors, secondary boot option is also provided.
I agree with Your considerations above.
Regards,
Yuri.
Hello Yuri,
Thank you for your quick response.
I was able to understand how work boot ROM and secondary image.
Best regards,
Ishii.