Support TI wl1837mod Wi-Fi module in Android 4.3_1.1.0 Kernel 3.0.35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support TI wl1837mod Wi-Fi module in Android 4.3_1.1.0 Kernel 3.0.35

Jump to solution
3,220 Views
fredwang
Contributor I

We have a project to support TI wl1837mod Wi-Fi module in iMX6 board.

From linux-2.6-imx.git - Freescale i.MX Linux Tree , I only found TI wl1837mod exist from kernel 3.10.17, not exist in kernel 3.0.35.

Is it possible to port TI wl1837mod into kernel 3.0.35. And is there standalone driver for it?

Since in WL18xx First Time Getting Started Guide (IMX6) - Texas Instruments Wiki , I saw demo kernel is 3.10.53.

Thanks for any hint.

Labels (2)
0 Kudos
Reply
1 Solution
2,672 Views
igorpadykov
NXP Employee
NXP Employee

HI Fred

one can look at wl18xx porting in kernel 3.0.35 at

wl18xx and iMX6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,673 Views
igorpadykov
NXP Employee
NXP Employee

HI Fred

one can look at wl18xx porting in kernel 3.0.35 at

wl18xx and iMX6

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
2,672 Views
fredwang
Contributor I

Thank you very much for your quickly reply. I will try TI wl18xx driver in 'backports' package.

0 Kudos
Reply