Support BT656 and BT1120 Output For i.MX6 DUAL

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support BT656 and BT1120 Output For i.MX6 DUAL

1,706件の閲覧回数
BESTFREESCALE
Contributor II

Dear Members

I will use VIDEO ADC(=ADV7393 Chip and DSIP0 Port ,but didn't find out Default DISP Pin Map for YCrCb to use without changing SW.

IPUx_DISPx_DAT1[23:16] <==>P[7:0] , DIX_PIN2 --> HSYNC, DIX_PIN3 --> VSYNC , DISP_CLK--> CLK

(Y[7]/C[7]~Y[0]C[0])

IPUx_DISPx_DAT1[15:08] / C[7:0] <==>P[7:0]

IPUx_DISPx_DAT1[23:16] / Y[8:0] <==>P[15:8]

, DIX_PIN2 --> HSYNC, DIX_PIN3 --> VSYNC , DISP_CLK--> CLK

But , EVM isn't using the interface above. I want to double-check which interface is default. 

Is there no problem?

Do you know link to get  applicaiton, SW Code, and others?

Please let me know

ラベル(5)
0 件の賞賛
返信
2 返答(返信)

1,378件の閲覧回数
jayaramks
Contributor III

Hi Kim,

Could you interface adv7393 to IMX6 successfully?

Regards,

Ram

0 件の賞賛
返信

1,378件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信