Hi,
We would like to know if it is possible to connect an eMMC device with I/O levels (VCCQ) of 1.8V.
If so, how the connection should be made? (suppose we're using uSDHC3 to connect an eMMC device)?
Thanks,
Amir.
Hello,
yes, it is possible to interface 1.8V eMMC with i.MX6.
When using uSDHC3 for it, NVCC_SD3 should feed via 1.8V
supply.
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------