Supplying NVCC_SDx with 1.8V in case of eMMC device with VCCQ of 1.8V

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Supplying NVCC_SDx with 1.8V in case of eMMC device with VCCQ of 1.8V

607 Views
erezamir
Contributor II

Hi,

We would like to know if it is possible to connect an eMMC device with I/O levels (VCCQ) of 1.8V.

If so, how the connection should be made? (suppose we're using uSDHC3 to connect an eMMC device)?

Thanks,

Amir.

0 Kudos
1 Reply

384 Views
Yuri
NXP Employee
NXP Employee

Hello,

  yes, it is possible to interface 1.8V eMMC with i.MX6.

When using uSDHC3 for it, NVCC_SD3 should feed via 1.8V

supply.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos