Suggestions on video amp ICs for use with RGB outputs of the i.MX53?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suggestions on video amp ICs for use with RGB outputs of the i.MX53?

1,519 Views
mjpandrews
Contributor I

I've been looking at TI, ST, Fairchild, ... for

* Single +3.3V or +5V supply op amps

* Able to drive a 50 Ohm or 75 Ohm coax cable

* Operating in the order of 75-100MHz bandwidth (HD mode goes to 30MHz I believe). To be used with a gain of 2 for impedance matching.

* Capable of buffering the RGB outputs without acting like a filter or introducing too much of it's own brand of noise, harmonics, etc.

* Rail-to-rail input or reasonably close, not too much overhead required. Per the i.MX53 spec I saw somewhere the video output ranges from 1.37Vmax to 1.24Vmin. Did I read that right?

* LOW power ... of course. Right up there with free.

* A 3-channel IC would save some board space and hopefully some change, but single or dual would be great

Any suggestions? Thanks.

Labels (1)
0 Kudos
Reply
2 Replies

1,429 Views
igorpadykov
NXP Employee
NXP Employee

Hi Mike

yes, video output ranges from 1.37Vmax to 1.24Vmin. There are many

video amp ICs om market and one can ask vendor support for choosing right part,

though from i.MX53 point, it may be not good placing high emi source near

processor sensitive circuits like 32KHz, 24MHz oscillator circuits and ddr.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,428 Views
mjpandrews
Contributor I

Thanks, Igor. I picked the LMH6601 from TI. Looks good.

Have a good night.

Regards,

Mike Andrews

Principal Electrical Design Engineer

mandrews@soundmetrics.com<mailto:mandrews@soundmetrics.com>

Direct 425-822-3001 x315

Mobile 206-390-8607

www.soundmetrics.com<http://www.soundmetrics.com/>;

11010 Northup Way

Bellevue, WA 98004

Main 425-822-3001

This message (including any attachments) may contain confidential and privileged information. If you are not the intended recipient, please notify the sender and delete all copies of the original message without using or disclosing it. Thank you.

0 Kudos
Reply