Suggest a board based on i.MX6 Solo for development.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Suggest a board based on i.MX6 Solo for development.

1,022件の閲覧回数
vipulkumar
Contributor III

Hi,

I need a i.MX6 Solo based board for the development purpose. I will use 

OS - Linux

Yocto - 1.6.1

I have the following requirements:

1. i.MX6 Solo
2. LVDS Display
3. CAN
4. Audio
5. RS485
6. RS232
7. RS422
Can anybody suggest the best board for the above requirements ? 
Also, please share the link and schematic of the board ?
0 件の賞賛
返信
1 返信

935件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Vipul

one can look at

NXP/Freescale i.MX 6 based Computer on Module - Apalis iMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信