May i know the Structure Flow of Imx8m mini evk board .
from the scratch . from the switch of modes having 4 modes .
when set to emmc mode what process is started and which .img file is started
when set to SD card mode what process is started and which .img file is started
when adding new perpherial such as wifi .GSM etc what all need to edit or config like drivers
how to support LVDS and in which path show i added the driver and which filr should i configure to enable LVDS support
Thanks in Advance
Regards
Ruban
解決済! 解決策の投稿を見る。
Hi Ruban
one can refer to sect.6.1 System Boot i.MX 8M Mini Applications Processor Reference Manual
For uboot/linux there is no specific i.mx flows, one can look at general web resources, like below
www.denx.de/wiki/pub/U-Boot/SummitELCE2015/U-Boot_startup_sequence.pdf
https://opensource.com/article/18/1/analyzing-linux-boot-process
Best regards
igor
Hi Ruban
one can refer to sect.6.1 System Boot i.MX 8M Mini Applications Processor Reference Manual
For uboot/linux there is no specific i.mx flows, one can look at general web resources, like below
www.denx.de/wiki/pub/U-Boot/SummitELCE2015/U-Boot_startup_sequence.pdf
https://opensource.com/article/18/1/analyzing-linux-boot-process
Best regards
igor