Structure Flow of Imx8m mini evk board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Structure Flow of Imx8m mini evk board

Jump to solution
569 Views
Ruban1
Contributor II

May i know the Structure Flow of Imx8m mini evk board .

from the scratch . from the switch of modes having 4 modes .

when set to emmc mode what process is started and which .img file is started 

when set to SD card mode what process is started and which .img file is started 

when adding new perpherial such as wifi .GSM etc what all need to edit or config like drivers

how to support LVDS and in which path show i added the driver and which filr should i configure to enable LVDS support

Thanks in Advance

Regards

Ruban

Labels (1)
0 Kudos
1 Solution
1 Reply
563 Views
igorpadykov
NXP Employee
NXP Employee
0 Kudos