Structure Flow of Imx8m mini evk board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Structure Flow of Imx8m mini evk board

ソリューションへジャンプ
1,213件の閲覧回数
Ruban1
Contributor II

May i know the Structure Flow of Imx8m mini evk board .

from the scratch . from the switch of modes having 4 modes .

when set to emmc mode what process is started and which .img file is started 

when set to SD card mode what process is started and which .img file is started 

when adding new perpherial such as wifi .GSM etc what all need to edit or config like drivers

how to support LVDS and in which path show i added the driver and which filr should i configure to enable LVDS support

Thanks in Advance

Regards

Ruban

ラベル(1)
0 件の賞賛
返信
1 解決策
1,206件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信
1 返信
1,207件の閲覧回数
igorpadykov
NXP Employee
NXP Employee
0 件の賞賛
返信