There's a strange offset on our status bar:
and the navigator bar. I changed the background colors to make it more clear. If I call getLocationOnScreen() on the StatusBarView it reports 0,0. Which clearly is wrong.
Changing the wallpaper will make it appear above the status bar until the screen is redrawn. The purple arrow points to a single line that also appears in the apps screen, but I think it's a symptom of the other error.
I'm pretty much lost of ideas. Anyone?
In landscape mode it looks like this:
 
					
				
		
Thomas
Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel
free to reply with an update to this discussion.
Thanks,
Yixing
 
					
				
		
No.
 
					
				
		
Thomas
I will branch your this discssion into an internal group and assign an engineer to look into it. Sorry for the delay.
Regards,
Yixing
 
					
				
		
 SergioSolis
		
			SergioSolis
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Thomas, which device are you using?, is it a sabre board?, and are you using the included LVDS or a different display?
 
					
				
		
http://www.spectralink.com/pivot/
It's based on the sabre board.
If I disable hardware acceleration for the status and navigation bar the problem is gone.
 
					
				
		
 daiane_angolini
		
			daiane_angolini
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		which hardware acceleration do you enable/disable in navigator bar to get this bug on/off? I mean 3d, 2d?
Does this happen only with LVDS? Or if you display on HDMI you can reproduce the same behavior?
I´m not sure you have already said that, but, please, let us know your resolution in any case :smileywink: