Sticky Bit error of i.MX6Solo with using debugger

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sticky Bit error of i.MX6Solo with using debugger

Jump to solution
1,740 Views
yuuki
Senior Contributor II

Dear All,

In our original board, we accessed the EIM_CS0 area(0x0800_0000-) by using JTAG.

However, when we access the EIM_CS0 area after a system Boot from SD, Sticky Bit error occurs.
Word access and double word access were tried, but it was the same result.

May I have any advice to evade this error?


Best Regards,
Yuuki

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
1,607 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

had you set CCM_CGPR6, CG5 for EIM clock enabling ?

Best regards

igor

View solution in original post

0 Kudos
Reply
2 Replies
1,608 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yuuki

had you set CCM_CGPR6, CG5 for EIM clock enabling ?

Best regards

igor

0 Kudos
Reply
1,607 Views
yuuki
Senior Contributor II

Dear igor-san,

Thank you very much for your support.

I found CG5 field of the CCM_CCGR6 register having been 00.

The problem was solved by setting this value to "11".

Best Regards,

Yuuki

0 Kudos
Reply