Stereoscopic camera video streaming in iMX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Stereoscopic camera video streaming in iMX6Q

476件の閲覧回数
mptech
Contributor I

I'm planning to design a stereoscopic camera which is using two OV5642 (parallel interface) image sensors. Two sensors are connected to iMX6Q IPU1 (parallel interface) and IPU2 (parallel interface). Suppose I can configure the two sensors simultaneously and using the same clock source. That means the state machines of both sensors are synchronized. In video streaming mode, Is iMX6Q possible to receiving both sensors data into system memory simultaneously with frame synchronization?

ラベル(1)
0 件の賞賛
0 返答(返信)