Hello everyone,
I'm sharing my experience bringing-up a TI Wilink Module (WL18xx) on iMX6 Linux 3.10.53
You can find a lot of information here: WL18xx - Texas Instruments Wiki
And iMX6 instructions here- WL18xx First Time Getting Started Guide (IMX6) - Texas Instruments Wiki
Hardware setup -- iMX6 communicates with WL18xx over SDIO (WiFI) and UART (Bluetooth).
On iMX6, the tricky part is correct connection of the UART lines, especially the RTS/CTS lines.
In DCE mode (default) the signals should be connected as follows:
WL18xx Module iMX6 Port
[Out] Pad 50 (BT_HCI_RTS) ----> UART_RTS
[In ] Pad 51 (BT_HCI_CTS) <---- UART_CTS
[Out] Pad 52 (BT_HCI_TX) ----> UART_RX
[In ] Pad 53 (BT_HCI_RX) <---- UART_TX
If the RTS/CTS lines are connected incorrectly, the BT driver won't be able to load.
Software setup-
You should have Linux 3.10.53 and a Root file-system ready.
(Make sure you don't have any uncommitted changes)
To build the WiFi drivers, follow the steps in WL18xx System Build Scripts - Texas Instruments Wiki
In the setup-env file :
TOOLCHAIN_PATH -- Either use your iMX6 toolchain, or leave as default (it worked for me).
ROOTFS -- Point to your root filesystem
KERNEL_PATH -- Point to you Linux kernel sources
KERNEL_VARIANT -- Set to 'imx-3.10.53' (This will apply patches to your kernel !)
Steps to build the WL18xx software:
git clone git://git.ti.com/wilink8-wlan/build-utilites.git
cd build-utilites/
cp setup-env.sample setup-env
<edit setup-env>
./build_wl18xx.sh init (This will take a long time)
./build_wl18xx.sh patch_kernel
The last step applies several patch to your kernel. The patches include updates to the sources files, configuration files, and device tree files.
If you use a different kernel configuration than imx_v7_defconfig, make sure to make the same kernel changes to your configuration.
Also, update your device tree files according to the patches.
In your device tree, make sure to setup the BT_EN_SOC, WLAN_EN_SOC, and WL_IRQ GPIOs correctly, and provide them in the correct nodes in the device tree.
Here's an example -
// BT and WiFI Enable [OUT]
MX6QDL_PAD_EIM_D16__GPIO3_IO16 0x13059 // BT_EN_SOC
MX6QDL_PAD_EIM_D17__GPIO3_IO17 0x13059 // WLAN_EN_SOC
MX6QDL_PAD_SD3_DAT4__GPIO7_IO01 0x13059 // WL_IRQ
wlan_en_reg: fixedregulator@2 {
compatible = "regulator-fixed";
regulator-name = "wlan-en-regulator";
regulator-min-microvolt = <1800000>;
regulator-max-microvolt = <1800000>;
/* WLAN_EN GPIO for this board – Bank4, pin7 */
gpio = <&gpio3 17 0>;
/* WLAN card specific delay */
startup-delay-us = <70000>;
enable-active-high;
};
kim {
compatible = "kim";
nshutdown_gpio = <80>; /* GPIO3_IO16 */
dev_name = "/dev/ttymxc2";
flow_cntrl = <1>;
baud_rate = <3000000>;
};
btwilink {
compatible = "btwilink";
};
&usdhc3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_usdhc3>;
no-1-8-v;
keep-power-in-suspend;
enable-sdio-wakeup;
vmmc-supply = <&wlan_en_reg>;
non-removable; /* non-removable is not a variable, the fact it is */
/* listed is all that is used by driver */
cap-power-off-card;
status = "okay";
#address-cells = <1>;
#size-cells = <0>;
wlcore: wlcore@0 {
compatible = "ti,wlcore";
reg = <2>;
interrupt-parent = <&gpio7>;
interrupts = <1 0>;
platform-quirks = <1>;
};
};
&uart3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart3>;
status = "okay";
/* enable rts/cts usage on uart3 */
fsl,uart-has-rtscts;
};
Now -- build you kernel -
make -j4 uImage modules dtbs
Install the modules in your root filesystem
make modules_install INSTALL_MOD_PATH=<rootfs path>
Now, run the last step in the Wilink build script:
./sudo_build_wl18xx.sh update R8.5
This will build and install the Wilink drivers and software in the root filesystem.
That's it! -- it should work. The wifi modules should load automatically when the kernel boots.
How to test?
WIFI -
> ifconfig wlan0 up
> iw wlan0 scan
(This should display a list of access points).
Bluetooth -
> hciconfig hci0 up
> hcitool scan
(This should scan for bluetooth devices).
Additional comments-
1. You can also use Linux 3.14.28, but you'll have to apply the patches manually.
2. If you have an issue with RTS/CTS, you can disable it. :
(a) Change flow_cntrl to <0> in kim.
(b) Change the baud rate to 115200 in kim.
(c) Remove fsl,uart-has-rtscts; in the uart node.
(d) Remove the CTS and RTS in the IOMUX
(e) Comment out line 208 in src/uim/uim.c (in the build-utilites folder)
ti.c_cflag |= CRTSCTS;
NOTE 1: Without RTS/CTS you must bring up the Bluetooth driver first
NOTE 2: You really should use RTS/CTS -- otherwise expect problems due to sync lost between host and module.
Good luck!
Hello Erez!
Thank you for so fast responce!
You were right - kim was mistakenly identified in the "regulators" field.
Now:
UIM SYSFS Node Found at /sys/./devices/soc0/kim.25/install
Starting uim-sysfs daemon.
uim:@ main
uim:install = /sys/./devices/soc0/kim.25/install
uim:dev_name = /sys/./devices/soc0/kim.25/dev_name
uim:baud_rate = /sys/./devices/soc0/kim.25/baud_rate
uim:flow_cntrl = /sys/./devices/soc0/kim.25/flow_cntrl
uim:install set previously...
uim:@ st_uart_config
uim: signal received, opening /dev/ttymxc4
uim:@ set_baud_rate
uim:set_baud_rate() done
uim:Setting speed to 3000000
uim:@ read_command_complete
uim: Command complete started
uim:@ read_hci_event
uim: read_hci_event
uim:Invalid response
At the end of bootlog:
uim:begin polling...
uim:poll broke due to event 10(PRI:2/ERR:8)
uim:read 0 from install
uim:@ st_uart_config
uim:Un-Installed N_TI_WL Line displine
uim:begin polling...
I thought that it might be a rfkill:
root@plaz-ilim:~# rfkill list
0: hci0: bluetooth
Soft blocked: yes
Hard blocked: no
root@plaz-ilim:~# rfkill unblock all
root@plaz-ilim:~# rfkill list
0: hci0: bluetooth
Soft blocked: no
Hard blocked: no
root@plaz-ilim:~# hci
hciattach hciconfig hciemu hcitool
root@plaz-ilim:~# hciconfig hci0 up
(stc): chnl_id list empty :4
(stk) : st_kim_start(stk) :ldisc_install = 1uim:poll broke due to event 10(PRI:2/ERR:8)
uim:read 1 from install
uim:@ st_uart_config
uim: signal received, opening /dev/ttymxc4
uim:@ set_baud_rate
uim:set_baud_rate() done
uim:Setting speed to 3000000
uim:@ read_command_complete
uim: Command complete started
uim:@ read_hci_event
uim: read_hci_event
uim:Invalid response
(stk) :ldisc installation timeout(stk) :ldisc_install = 0
(stk) : timed out waiting for ldisc to be un-installed(stk) :ldisc_install = 1
/* = 0 and = 1 5 times*/
(stk) : timed out waiting for ldisc to be un-installedBluetooth: st_register failed -22
Can't init device hci0: Input/output error (5)
I don't know what to do with this...
Regarding the "update R8.5", I have a compilation error because it can't apply 0001-completion-remove-reinit_completion-decleration.patch and i'm forced to apply it manually,
If i do a "update R8.5", my changes overwrites by script and it is a vicious circle.
Hi Erez,
Its ready explains most of the things, really helpful document.
Thanks
Saurabh