I have a Digi i.MX6UL with Yocto running on it and it does not support iptables. I was told I needed to rebuild the image and add the package for iptables. Anyone have step by step on how to do this? I have started with Yocto Project Quick Build to see how close I can get to having at least the environment up. This is the steps from Digi to build the development environment ConnectCore 6UL SBC Pro | DEY-2.4
Hello Don Osmond,
The Yocto BSP has an iptables package available, which can be added to an image by adding the following line on the conf/local.conf file:
IMAGE_INSTALL_append = “ iptables”
However, I’m not familiar with Digi’s BSP. You can see the available packages inside a Yocto envionment by running:
$ bitbake -s
For specific details on Digi’s BSP I would recommend looking at their support forums.
I hope this helps!
Regards,
Thanks for the suggestion. I am not able to run a bitbake on this image either. When I tried to use iptables with the following: I received an error.
root@ccimx6ulsbc:~# iptables -t nat -A PREROUTING -i eth1 -m tcp --dport 5000 -j DNAT --to- 208.104.29.77
modprobe: module ip_tables not found in modules.dep iptables v1.6.1: can't initialize iptables table `nat': Table does not exist (do you need to insmod?) Perhaps iptables or your kernel needs to be upgraded.
root@ccimx6ulsbc:~#
It seems you need to recompile Linux with IP tables and its dependencies enabled.
Agreed and that is the question. What steps do I need to add the proper package for iptables and build the new image?