State of iMX28 in Linux 3.x Kernels?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

State of iMX28 in Linux 3.x Kernels?

1,782件の閲覧回数
mwill
Contributor I

Greetings all,

Im having a bunch of performance issues using recent 3.x linux kernels (slow uSD, USB, linuxfb, etc performance).

It also appears cpufreq, powersaving, etc functions are not availiable.

Is there any Freescale support/maintenance of the iMX28 in the 3.x kernels, or would i be better off moving back to 2.6.35 with related Freescale patches?

Thanks in advance,

ラベル(2)
0 件の賞賛
返信
5 返答(返信)

1,497件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Mark,

Which kernel version did you use? It would be nice if you could report the issues you noticed in the linux-arm-kernel mailing list, so that people could be aware of them and eventually fix them.

0 件の賞賛
返信

1,497件の閲覧回数
mwill
Contributor I

I'm using 3.17.4, and have tried a few previous 3.x versions as well.

By "people" im guessing you mean the community, and not Freescale?

0 件の賞賛
返信

1,497件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

Yes, I mean the community. If you report the issues in details in the mailing lists, then maybe someone can try to fix them.

1,497件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Mark

I think you are right, since officially supported only releases located

on Freescale i.MX product web pages, like below

i.MX28 Evaluation Kit|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,497件の閲覧回数
mwill
Contributor I

So does that mean Freescale has stopped maintaining Linux support for the iMX2x?

0 件の賞賛
返信