Hi all,
Our custom board is using i.mX7D and PMIC PF3000 as below:
i.MX7D : MCIMX7D7DVM10SD
PMIC : MC32PF3000A1EP
We found the below GPIOs drive level high immediately after its gpio power rail up, even when the gpio is pull-down by a 200-ohm resistor.
Exactly it is a 4ms high pulse. Please see the attach file for more detail.
Note that the power-on-reset is asserting, and the gpio are pull-down by a 1k resistor.
power-rail : NVCC_I2C
Pad: I2C3_SDA (ball K6)
I2C4_SCL (ball L1)
My questions are below:
1. Does the gpio drive high level during its group power up meet the i.MX7D specs ?
2. These GPIO are assumed as three-state during power up, is this right?
3. Unexpected high level output will conflict with the connected device. This phenomenon are seen on only 3 boards. On the other boards, these GPIO keep low during power up.
Do you have any idea in this case?
Best Regards
Nhat