Startup for PF1550+i.MX6ULL power-on

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Startup for PF1550+i.MX6ULL power-on

944 Views
yuji_matsunami
Contributor II

Hi,
We would like to use PF1550 for our implementation with i.MX6ULL.
The SW1 starts at the same timing as the SW1 against VLDO3 at power-on. (Difference less than 0.1ms)
Looking at the following Figure 27 on the PF1550 datasheet, I think the output is delayed by tD3(1.5 -6.0ms).
Is the behavior when the power is turned on different from the datasheet?
The PWRON pin is always High and the STANDBY pin is always Low.

Labels (1)
0 Kudos
3 Replies

937 Views
john_phillippe
NXP Employee
NXP Employee

I don't quite understand your question.  Are you seeing behavior on your device that is different than what is described in the datasheet?

0 Kudos

929 Views
yuji_matsunami
Contributor II

There is no power up delay difference between VLDO3 and SW1.(Difference less than 0.1ms)

0 Kudos

924 Views
john_phillippe
NXP Employee
NXP Employee

In the case you highlighted there are three periods of Td3 (0.5ms typ) which would give a typical delay of 1.5ms if OTP_SEQ_CLK_SPEED=0, and 6ms total delay if OTP_SEQ_CLK_SPEED=1.

 

0 Kudos