Startup Timing Diagram with non LDO Bypass

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Startup Timing Diagram with non LDO Bypass

1,346 次查看
ko-hey
Senior Contributor II

Hi all

I have a question about detailed power-up sequence.

In following guide, it shows startup timing diagram in LDO Bypass mode.

But there is no diagram in non LDO Bypass mode.

http://cache.nxp.com/files/32bit/doc/user_guide/IMX6SLHDG.pdf

Please provide me the diagram in non LDO Bypass mode.

Ko-hey

标签 (2)
标记 (1)
0 项奖励
回复
2 回复数

1,265 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Please  follow the Datasheet recommendations, as discussed in the following

thread Re: About Power sequence in i.MX6SL.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,265 次查看
ko-hey
Senior Contributor II

Hi

There are no description about non bypass mode so user have to follow the datasheet recommendation.

Is it correct ?

Ko-hey

0 项奖励
回复