Hi Ankur
some info for standby (echo standby > /sys/power/state) :
VDDD - 10mA, VDDA - 5mA,VDDIO - 15mA,VDD1P5 - 5mA
For case powering from 5V input you can recalculate power consumption,
using voltage difference between 5V and LDOs.
Case 2 never measured, seems it is the same as case 1.
Best regards
chip
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thank you Chipexpert for sharing this information.
If I understood it correctly, which this I can calculate the power consumption on prototype using 5V. But I would like to know from Freescale, what is the best that can be achieved in Standby mode using I.MX28?
The problem is currently with Standby mode our prototype consumes around 1 Watt and our product requirement is below 0.6 Watt. Now, I would like to know if I.MX28 in standby mode with 5V does actually goes below 0.6 Watt or not.
Regards,
Ankur
I am afraid that data which you require, were not measured.
Best regards
chip