Standalone Boot loader for imxrt1060

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Standalone Boot loader for imxrt1060

1,417件の閲覧回数
palak_shah1
Contributor II

Hi,

We have an imxrt1060 based custom board. We are running our own application on it so far and its OK. 

Either I use a jtag to download the code or flash the code on the QSPI flash using MCU boot utility. 

Now, there is a need to add a boot loader. I have seen the SDK examples - evkimxrt_flashloader and imxrt_mcuboot_opensource. I have also looked at the SBL and SFW source code, but these are huge sources and has a lot of functionality. 

I am looking for a stand alone boot loader which is its own application that i can flash on the QSPI flash. 

Is there any example or code available that I can use or look at?

Thanks,

Palak

0 件の賞賛
返信
3 返答(返信)

1,409件の閲覧回数
palak_shah1
Contributor II

Can someone please reply to this?

0 件の賞賛
返信

1,401件の閲覧回数
palak_shah1
Contributor II

Hi,

I really want to know if we have any stand alone boot loader examples for imxrt1060 based. Any input is appreciated. 

Thanks,

Palak

0 件の賞賛
返信

1,379件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @palak_shah1 

I hope you are doing well, 

I think that you could refer to the  AN12604 Implement second bootloader on i.MXRT10xx series (i.MX RT1050, i.MX RT1020, and i.MX RT1060 are covered in the app note)

This application note provides information about the basic elements to implement a secondary bootloader. The software for this application  note is here AN12604 software   

Do not hesitate to let me know if there is anything else we should discuss.

Many thanks for your patience.

Diego.

0 件の賞賛
返信