Stable Yocto Image for i.MX8M Plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Stable Yocto Image for i.MX8M Plus

1,754 次查看
BrunoSenzio
Contributor III

Hello,

I just received a board from an SBC manufacturer, however, when I flash media like the eMMC, SD or USB and boot their yocto image, it does not load properly, receiving Kernel alarms or getting stuck at the loading screen with prompts like 

cfg80211: failed to load regulatory.db
 
Is there any resource I could use to get a stable Yocto running on my board?
 
Thanks in advance
0 项奖励
回复
3 回复数

1,735 次查看
BrunoSenzio
Contributor III

Yes I have different HW. I will have to wait and see...

0 项奖励
回复

1,742 次查看
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Bruno,

 

Please download the demo image from our web, https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-...

If you have other hardware than EVK, you must check with the vendor if they have a demo image.

 

Regards

 

 

0 项奖励
回复

1,624 次查看
colinbroderick
Contributor III

Could you provide a little more information on which file you're referring to? It's not clear to me which is most appropriate.

I'm currently downloading the one labelled L5.10.35_2.0.0_MX8MP. Is that a full bootable image?

Thanks

0 项奖励
回复