Stable Yocto Image for i.MX8M Plus

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stable Yocto Image for i.MX8M Plus

1,743 Views
BrunoSenzio
Contributor III

Hello,

I just received a board from an SBC manufacturer, however, when I flash media like the eMMC, SD or USB and boot their yocto image, it does not load properly, receiving Kernel alarms or getting stuck at the loading screen with prompts like 

cfg80211: failed to load regulatory.db
 
Is there any resource I could use to get a stable Yocto running on my board?
 
Thanks in advance
0 Kudos
Reply
3 Replies

1,724 Views
BrunoSenzio
Contributor III

Yes I have different HW. I will have to wait and see...

0 Kudos
Reply

1,731 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Bruno,

 

Please download the demo image from our web, https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/evaluation-kit-...

If you have other hardware than EVK, you must check with the vendor if they have a demo image.

 

Regards

 

 

0 Kudos
Reply

1,613 Views
colinbroderick
Contributor III

Could you provide a little more information on which file you're referring to? It's not clear to me which is most appropriate.

I'm currently downloading the one labelled L5.10.35_2.0.0_MX8MP. Is that a full bootable image?

Thanks

0 Kudos
Reply