Spi slave receive word from previous transfer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Spi slave receive word from previous transfer

1,792件の閲覧回数
s233199
Contributor II

Hello, I have a problem with my spi slave driver. The master sends 10 words, and in my test application I want to receive only 8 of them. When I run my test application I receive the 8 words correctly. But when I run the test the next times, I receive as first word the 9th word, and then the 1-2-3-4-5-6-7 words.Trying the test again, I receive 8-1-2-3-4-5-6-7, so the first word is always the next I should have received in the previous test.

After each transfer I reset the receive fifo, so I do not understand why I read the 9th word. Is it possible that I have to reset other registers?

I am using the board i.mx8qmlpddr4arm2 with Yocto.

Thank you for the answers!

0 件の賞賛
返信
3 返答(返信)

1,612件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

I suggest you use the ECSPI test that we have in our Linux BSP. You can find it in the below path:

# cd /unit_tests/ECSPI

There we do have a spi example.

Hope this could help you.

Best regards,

Diego.

0 件の賞賛
返信

1,612件の閲覧回数
s233199
Contributor II

Thank you for the answer. My board (i.mx8 quad max lpddr4 arm2) is using LPSPI. I think when I stop receiving, something remains in the shift register, and this is read in the next transfer. How can I clean the shift register? I am only able to reset the receive fifo, but not the entire shift register.

0 件の賞賛
返信

1,612件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello

I apologize for the delay.

Unfortunately, the i.MX8QM is still in preproduction, we cannot support this product or guarantee anything since the information can be subject to change. I apologize for the inconveniences this could give you.

Best regards,

Diego.

0 件の賞賛
返信