Specification of DRAM_SDCLK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Specification of DRAM_SDCLK

1,040 次查看
eishishibusawa
Contributor III

Dear Sir

 

I want to confirm the specification of SDCLK for i.MX6Dual.

 

It is described at P5 in IMX6DQAEC Rev4 as following.

External memory interfaces:

 16-bit, 32-bit, and 64-bit DDR3-1066

 

I understand that it supports up to 533MHz as SDCLK.

I cannot find the minimum value for the SDCLK.

 

Q1.

What is the minimum value for SDCLK?

 

Q2.

Is it able to use DDR3-800(SDCLK=400MHz)?

 

Best Regards,

Eishi SHIBUSAWA

标签 (2)
0 项奖励
回复
1 回复

915 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Jedec specs provide data for the following configurations :

DDR3-800, DDR3-1066, DDR3-1333, DDR3-1600, DDR3-1866, DDR3-2133.

According to the specs Minimum Clock Cycle Time (DLL off mode) is 8 ns.

  So, DDR3-800 is minimal frequency configuration from the recommended ones.

It is supported by i.MX6, assuming timing parameters should be set for 400 MHz. 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复