Sourcing image from memory of ISI module in iMX8QXP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sourcing image from memory of ISI module in iMX8QXP

Jump to solution
1,777 Views
Kazuma_Sasaki
Senior Contributor I

Hello,

Latest reference manual (IMX8DQXPRM.pdf Rev.0) mentioned following steps which copying image data from memory to ISI module. However, several registers have been missed in register memory map. Are CHNL_IN_BUF_ADDR, CHNL_IN_BUF_PITCH and CHNL_MEM_RD_CTRL registers remaining in latest device (C0 rev)?

I think it is a typo. Will it be revised in nearly future? 

15.4.1.7.7 Sourcing Image from Memory
A channel can be configured to read image from memory in two cases:
• During Blending De-interlace, hardware controlled memory reads occur.

  Refer to Image Deinterlacing section for more details.
• Software controlled memory read. This section details the configuration required for software controlled memory     reads. Please follow the channel initialization steps prior to configuring the memory image read on a channel.

   The steps to configure channel are:
• Configure the memory address from where the image is to be sourced in the CHNL_IN_BUF_ADDR[ADDR].
• Configure the line and frame pitch in the CHNL_IN_BUF_PITCH register.
• Configure the read image format in the CHNL_MEM_RD_CTRL[IMG_TYPE] field.
• Complete the initialization of other blocks and interrupts for channel 0 and set CHNL_CTRL[CHNL_EN] = 1.
• Set the CHNL_MEM_RD_CTRL[READ_MEM] = 1 to enable reading of frame from memory.
• Wait for CHNL_STS[MEM_RD_DONE] interrupt to set before initiating a new image read.

  When this interrupt occurs, set CHNL_MEM_RD_CTRL[READ_MEM]

Copy from latest reference manual (Rev.0)

pastedImage_8.png

Copy from old reference manual (Rev.E)

pastedImage_9.png

Linux BSP definition (L4.14.98_2.3.0_ga / mxc-isi-hw.h)

pastedImage_10.png

Best Regards,

Kazuma Sasaki.

Tags (2)
1 Solution
1,679 Views
Yuri
NXP Employee
NXP Employee

Hello,

   it appears these registers have been removed by mistake, will log this and they should

be added back in to the next version.

Regards,

Yuri.

View solution in original post

0 Kudos
Reply
2 Replies
1,680 Views
Yuri
NXP Employee
NXP Employee

Hello,

   it appears these registers have been removed by mistake, will log this and they should

be added back in to the next version.

Regards,

Yuri.

0 Kudos
Reply
1,679 Views
Kazuma_Sasaki
Senior Contributor I

Hi Yuri,

I appreciate your support. I got it. 

Best Regards,
Kazuma Sasaki.