Sometimes Failed to detect NAND on i.MX6UL in u-boot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sometimes Failed to detect NAND on i.MX6UL in u-boot

1,801 Views
dhvanil_patel1
Senior Contributor I

Hi,

I am working on a board based on i.MX6UL. I am using "MT29F8G08ABABA" nand on i.mx6ul. I am using u-boot version "2015.04". Sometimes I am facing an issue that No NAND device is detected and sometime device is detected.

Can you help us to resolve this issue ASAP ?

Is this issue related to Fail to boot from NAND flash | NXP Community  ?

Waiting for response.

///////  Failed to detect NAND log ////////////////////////////

U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Aug 10 2016 - 11:30:25)

CPU:   Freescale i.MX6UL rev1.0 at 396 MHz

CPU:   Temperature 24 C

Reset cause: POR

Board: MX6UL Volansys BR

I2C:   ready

DRAM:  256 MiB

PMIC: PFUZE3001 DEV_ID=0x31 REV_ID=0x11

NAND:  0 MiB                         // No Nand device is detected

MMC:   Inside FSU_config 0

FSL_SDHC: 0

*** Warning - readenv() failed, using default environment       // Failed to read environment from NAND

In:    serial

Out:   serial

Err:   serial

Net:   FEC0

Normal Boot

Hit any key to stop autoboot:  0

=> set ethaddr 70:B3:D5:9A:E0:06

=> boot

no devices available

no devices available

Bad Linux ARM zImage magic!

=>

/////////////////////////////////////////

Working log

//////////////////

U-Boot 2015.04-imx_v2015.04_3.14.52_1.1.0_ga+g6cf684a (Aug 10 2016 - 11:30:25)

CPU:   Freescale i.MX6UL rev1.0 at 396 MHz

CPU:   Temperature 33 C

Reset cause: POR

Board: MX6UL Volansys BR

I2C:   ready

DRAM:  256 MiB

PMIC: PFUZE3001 DEV_ID=0x31 REV_ID=0x11

NAND:  1024 MiB

MMC:   Inside FSU_config 0

FSL_SDHC: 0

*** Warning - bad CRC, using default environment

In:    serial

Out:   serial

Err:   serial

Net:   FEC0

Normal Boot

Hit any key to stop autoboot:  0

NAND read: device 0 offset 0x4000000, size 0x800000

8388608 bytes read: OK

NAND read: device 0 offset 0x5000000, size 0x100000

1048576 bytes read: OK

Kernel image @ 0x80800000 [ 0x000000 - 0x55abd0 ]

## Flattened Device Tree blob at 83000000

   Booting using the fdt blob at 0x83000000

   Using Device Tree in place at 83000000, end 8300a692

switch to ldo_bypass mode!

Starting kernel ...

/////////////////////////////////////////////////////

-

Thanks,

Dhvanil Patel

Labels (3)
0 Kudos
Reply
3 Replies

1,165 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dhvanil

this may be caused by signal integrity issues, so one can inspect

nand lines with oscilloscope and tweak its drive strength. Also one can

try to slightly change nand voltage.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,165 Views
dhvanil_patel1
Senior Contributor I

Hi igor,

Thank you for your prompt response.

Can you please elaborate more on this signal integrity issue? Which nand single should I inspect ? All data lines or control signals ? The NAND voltage is 3.3V. We are not able to change this voltage.

-

Dhvanil Patel

0 Kudos
Reply

1,165 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dhvanil

yes all data lines or control signals.

Best regards

igor

0 Kudos
Reply