Some trouble between ChipIdea and audio Gadget‏

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some trouble between ChipIdea and audio Gadget‏

1,503件の閲覧回数
ise1
Contributor III

Dear All ,
 

I'm working on IMX6 SabreLite (with a 3.10.53 kernel) and have some trouble in using the HNP protocol in order to switch the role host/device of my boards.
I have set some configurations in menuconfig like "USB 2.0 OTG FSM Implementation", "ChipIdea HighSpeed Dual Role Controller", "ChipIdea device controller" and "ChipIdea host controller". I have used this uImage in my two sabreLite. But I'm stuck in the step 2 (from this document:
https://www.kernel.org/doc/Documentation/usb/chipidea.txt). After loading g_audio in my two sabreLite and plugging the cable (microA – microB), there is an error “ci_hdrc.0 request length too big for isochronous  snd_uac2.0 1116 Error”.

And even after running aplay command, I still got this error and there is no sound getting out of the jack port. Are there any incompatibility between ChipIdea and Audio Gadget ?

Are there someone who has this trouble ? How can I fix it ?

Thanks

0 件の賞賛
返信
1 返信

1,320件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi,

As you are using a SabreLite board, we would suggest to direct your question to Boundary Devices webpage:

http://boundarydevices.com/product/sabre-lite-imx6-sbc/

Best regards!

/Carlos

0 件の賞賛
返信