Some questions from newbie for iMX8MP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Some questions from newbie for iMX8MP

692 次查看
nnxxpp
Contributor IV

I am a newbie with NXP board. I have iMX8MP board.

I know that it can run Android and Linux (Linux is default built-in OS in EMMC and we can run without need to set up anymore). If we want to run Android, we need to rebuild with Android OS.

In the past, I used MIMXRTxxxx board and I could download SDK for this board. I used MCUXpresso IDE and Ubuntu. I can download SDK for MIMXRTxxxx in the format .zip and I could import it into the SDK. But for iMX8MP, I see that there is not SDK option for MCUXpresso IDE and the file is in .tar.gz (not .zip file). It only supports for MCUXpresso Vscode and ARM GCC. How can I use this SDK in MCUXpresso IDE?

Moreover, I see that in the SDK download plane, there is option for FreeRTOS. I am confused about it. It means that we can use only one OS for iMX8MP at one time (one from FreeRTOS, Adnroid or Linux). Is that right?

I saw that FreeRTOS is for M7 core? If we use FreeRTOS, we can not use A53 cores (more powerfull than M7 core) at one time. is that right?

How can I install FreeRTOS for iMX8MP? and how I can use SDK .tar.gz in the above comment in FreeRTOS? I am newbie in the embedded field, so something is confused.

The last question. If I want to run tflite and NPU tflite with FreeRTOS on iMX8MP. What I need to start? (before with MIMXRTxxxx, I can run debug tflite cifar10 application with example from SDK)

Sorry for many questions. Thank you

标签 (1)
0 项奖励
回复
1 回复

634 次查看
June_Lu
NXP TechSupport
NXP TechSupport

Please kindly download the MCUXprosso SDK

Welcome | MCUXpresso SDK Builder, there is no MCUXpresso IDE compatible SDK  you could not use MCUXpresso IDE

M core and A core could run different OS.

From the https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software:IMX-SW you could get the generally SW support.

For the A core, FreeRTOS is not listed in the Supported Operating Systems for Arm® Cortex®-A.

0 项奖励
回复