Some parts of the camera frame are green

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some parts of the camera frame are green

533 Views
gavincho
Contributor I

Hi,

My environment is i.MX8X + one MIPI-CSI2 digital camera (resolution is 2M).

I modify max9286 driver to let it support another serializer (MAX96705) and connect with another camera sensor.

When I use yavta to capture the frame, 1/3 to the right of the frame is green as below.

pastedImage_5.jpg

I want to know if i.MX8X MIPI CSI-2 can support 1080p or not.

PS:

From imx-yocto-L4.14.98_2.0.0_ga Linux release notes.pdf, we can see that it says MIPI CSI camera can support up to 1080p.

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

Thanks.

0 Kudos
1 Reply

409 Views
b36401
NXP Employee
NXP Employee

Actually green screen usually means some hardware issue like no signal from camera.
So in your case I suppose that there is no data from camera at this 1/3.
Possibly actual horizontal resolution of camera does not match expected resolution.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos