Some issues with booting with Image (Ubuntu Xenial 16.04 ) on i.MX6QP

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Some issues with booting with Image (Ubuntu Xenial 16.04 ) on i.MX6QP

16,460 次查看
erikraynolds
Contributor IV

Dears,

I've installed Ubuntu LXDE & MATE 16.04 per https://community.nxp.com/docs/DOC-330147 instructions onto i.MX6QP.

I have those Ubuntu images 16.04 LTS Xenial from

I got them that booting on NXP i.MX6QP device on Sabre AI board and can start GUI with "stratx" but still some issues I wan to get that working properly:

Here is "boot log":

    Welcome to Ubuntu 16.04.1 LTS!

    systemd[1]: Set hostname to <lubuntu>.
    usb 1-1.2: new low-speed USB device number 3 using ci_hdrc
    input: DELL DELL USB Laser Mouse as /devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb1/1-1/1-1.2/1-1.2:1.0/0003:046D:C063.0001/input/input5
    hid-generic 0003:046D:C063.0001: input: USB HID v1.10 Mouse [DELL DELL USB Laser Mouse] on usb-ci_hdrc.0-1.2/input0
    usb 1-1.3: new low-speed USB device number 4 using ci_hdrc
    systemd[1]: Created slice System Slice.
    [  OK  ] Created slice System Slice.
    systemd[1]: Reached target Slices.
    [  OK  ] Reached target Slices.
    systemd[1]: Listening on fsck to fsckd communication Socket.
    [  OK  ] Listening on fsck to fsckd communication Socket.
    systemd[1]: Reached target Encrypted Volumes.
    input: Dell Dell QuietKey Keyboard as /devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb1/1-1/1-1.3/1-1.3:1.0/0003:413C:2106.0002/input/input6
    [  OK  ] Reached target Encrypted Volumes.
    systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    hid-generic 0003:413C:2106.0002: input: USB HID v1.10 Keyboard [Dell Dell QuietKey Keyboard] on usb-ci_hdrc.0-1.3/input0
    systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
    [  OK  ] Listening on /dev/initctl Compatibility Named Pipe.
    systemd[1]: Created slice system-systemd\x2dfsck.slice.
    [  OK  ] Created slice system-systemd\x2dfsck.slice.
    systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    systemd[1]: Started Read required files in advance.
    [  OK  ] Started Read required files in advance.
    systemd[1]: Starting Restore / save the current clock...
             Starting Restore / save the current clock...
    systemd[1]: Starting Create list of required static device nodes for the current kernel...
             Starting Create list of required st... nodes for the current kernel...
    systemd[1]: Starting Nameserver information manager...
             Starting Nameserver information manager...
    systemd[1]: Starting Set console keymap...
             Starting Set console keymap...
    systemd[1]: Set up automount Arbitrary Executable File Formats File System Automount Point.
    [  OK  ] Set up automount Arbitrary Executab...ats File System Automount Point.
    systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    systemd[1]: Starting Journal Service...
             Starting Journal Service...
    systemd[1]: Mounting Debug File System...
             Mounting Debug File System...
    systemd[1]: Reached target Swap.
    [  OK  ] Reached target Swap.
    systemd[1]: Mounted Debug File System.
    [  OK  ] Mounted Debug File System.
    systemd[1]: systemd-modules-load.service: Main process exited, code=exited, status=1/FAILURE
    systemd[1]: Failed to start Load Kernel Modules.
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    systemd[1]: systemd-modules-load.service: Unit entered failed state.
    systemd[1]: systemd-modules-load.service: Failed with result 'exit-code'.
    systemd[1]: ureadahead.service: Main process exited, code=exited, status=5/NOTINSTALLED
    systemd[1]: ureadahead.service: Unit entered failed state.
    systemd[1]: ureadahead.service: Failed with result 'exit-code'.
    systemd[1]: Started Restore / save the current clock.
    [  OK  ] Started Restore / save the current clock.
    systemd[1]: Started Create list of required static device nodes for the current kernel.
    [  OK  ] Started Create list of required sta...ce nodes for the current kernel.
    systemd[1]: Started Set console keymap.
    [  OK  ] Started Set console keymap.
    systemd[1]: Started Nameserver information manager.
    [  OK  ] Started Nameserver information manager.
    systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
             Starting Create Static Device Nodes in /dev...
             Starting Apply Kernel Variables...
             Mounting FUSE Control File System...
    [  OK  ] Mounted FUSE Control File System.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [  OK  ] Started Apply Kernel Variables.
             Starting udev Kernel Device Manager...
    [  OK  ] Started udev Kernel Device Manager.
             Starting Remount Root and Kernel File Systems...
    [  OK  ] Started Remount Root and Kernel File Systems.
             Starting Flush Journal to Persistent Storage...
             Starting Load/Save Random Seed...
             Starting udev Coldplug all Devices...
    [  OK  ] Reached target Local File Systems (Pre).
    [  OK  ] Started Load/Save Random Seed.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started udev Coldplug all Devices.
    [  OK  ] Started Dispatch Password Requests to Console Directory Watch.
    DBG sensor data is at 7f010188
    [ TIME ] Timed out waiting for device dev-mmcblk0p1.device.
    [DEPEND] Dependency failed for /boot.
    [DEPEND] Dependency failed for Local File Systems.
    [DEPEND] Dependency failed for File System Check on /dev/mmcblk0p1.
             Starting Set console font and keymap...
    [  OK  ] Stopped Trigger resolvconf update for networkd DNS.
    [  OK  ] Stopped Network Manager.
    [  OK  ] Stopped Daily apt activities.
    [  OK  ] Closed Avahi mDNS/DNS-SD Stack Activation Socket.
    [  OK  ] Closed CUPS Scheduler.
    [  OK  ] Stopped target OEM Configuration.
    [  OK  ] Stopped End-user configuration after initial OEM installation.
    [  OK  ] Started Stop ureadahead data collection 45s after completed startup.
    [  OK  ] Closed D-Bus System Message Bus Socket.
    [  OK  ] Stopped Daily Cleanup of Temporary Directories.
    [  OK  ] Reached target Timers.
    [  OK  ] Stopped Permit User Sessions.
             Starting Set console scheme...
    [  OK  ] Stopped getty on tty2-tty6 if dbus and logind are not available.
    [  OK  ] Closed Socket activation for snappy daemon.
    [  OK  ] Stopped Save/Restore Sound Card State.
    [  OK  ] Closed Unix socket for apport crash forwarding.
    [  OK  ] Stopped Manage Sound Card State (restore and store).
    [  OK  ] Stopped target Basic System.
    [  OK  ] Reached target Paths.
    [  OK  ] Closed UUID daemon activation socket.
    [  OK  ] Stopped target System Initialization.
    [  OK  ] Started Emergency Shell.
    [  OK  ] Reached target Emergency Mode.
             Starting Tell Plymouth To Write Out Runtime Data...
             Starting LSB: AppArmor initialization...
             Starting Create Volatile Files and Directories...
    [  OK  ] Reached target Sockets.
    [  OK  ] Started Set console font and keymap.
    [  OK  ] Started Set console scheme.
    [  OK  ] Started Tell Plymouth To Write Out Runtime Data.
    [  OK  ] Started Create Volatile Files and Directories.
    [  OK  ] Started LSB: AppArmor initialization.
    [  OK  ] Started ifup for eth0.
    [  OK  ] Reached target Network.
             Starting Update UTMP about System Boot/Shutdown...
    [  OK  ] Reached target System Time Synchronized.
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    Welcome to emergency mode! After Give root password for maintenance
    (or press Control-D to continue):
    sulogin: failed to execute /bin/bash  : No such file or directory
    #
    # startx
    X.Org X Server 1.18.4
    Release Date: 2016-07-19
    X Protocol Version 11, Revision 0
    Build Operating System: Linux 4.2.0-42-generic armv7l Ubuntu
    Current Operating System: Linux lubuntu 4.1.15 #1 SMP PREEMPT Tue Nov 15 12:24:15 CET 2016 armv7l
    Kernel command line: console=ttymxc3,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
    Build Date: 14 September 2016  03:34:19PM
    xorg-server 2:1.18.4-0ubuntu0.1 (For technical support please see http://www.ubuntu.com/support)
    Current version of pixman: 0.33.6

          Before reporting problems, check http://wiki.x.org
            to make sure that you have the latest version.
    Markers: (--) probed, (**) from config file, (==) default setting,
            (++) from command line, (!!) notice, (II) informational,
            (WW) warning, (EE) error, (NI) not implemented, (??) unknown.
    (==) Log file: "/var/log/Xorg.0.log", Time: Thu Apr 21 10:42:14 2016
    (==) Using system config directory "/usr/share/X11/xorg.conf.d"
    modprobe: FATAL: Module g2d_23 not found in directory /lib/modules/4.1.15


 issue 1)

systemd[1]: Failed to start Load Kernel Modules.
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    systemd[1]: systemd-modules-load.service: Unit entered failed state.
    systemd[1]: systemd-modules-load.service: Failed with result 'exit-code'.
    systemd[1]: ureadahead.service: Main process exited, code=exited, status=5/NOTINSTALLED
    systemd[1]: ureadahead.service: Unit entered failed state.
    systemd[1]: ureadahead.service: Failed with result 'exit-code'.

Issue 2)

[ TIME ] Timed out waiting for device dev-mmcblk0p1.device.
    [DEPEND] Dependency failed for /boot.
    [DEPEND] Dependency failed for Local File Systems.
    [DEPEND] Dependency failed for File System Check on /dev/mmcblk0p1.

Issue 3)

    Welcome to emergency mode! After Give root password for maintenance
    (or press Control-D to continue):
    sulogin: failed to execute /bin/bash  : No such file or directory


Issue 4)

    modprobe: FATAL: Module g2d_23 not found in directory /lib/modules/4.1.15

If you can advice me how to correct it.

Thank you very much!

标记 (2)
0 项奖励
回复
20 回复数

10,056 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Erik,

The issue 3 is result of issue 2. The problem of issue 2 should be in the fstab. Try to change in file /etc/fstab device /dev/mmcblk0p1 to /dev/sda1. It can be slightly different, it depend on what you will find in the /etc/fstab.

The issue 4 is common log message, but it is not important and you can ignore it.

For the issue 1. You can start with repairing issue 2 and if the problem will continue send me log from command "systemctl status systemd-modules-load.service".

Radim.

0 项奖励
回复

10,056 次查看
erikraynolds
Contributor IV

change in file /etc/fstab device /dev/mmcblk0p1 to /dev/sda1

it seems issues prevails ...

Welcome to Ubuntu 16.04.1 LTS!

systemd[1]: Set hostname to <lubuntu>.
systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
systemd[1]: Set up automount Arbitrary Executable File Formats File System Automount Point.
[ OK ] Set up automount Arbitrary Executab...ats File System Automount Point.
systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
systemd[1]: Created slice system-systemd\x2dfsck.slice.
[ OK ] Created slice system-systemd\x2dfsck.slice.
systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
systemd[1]: Listening on fsck to fsckd communication Socket.
[ OK ] Listening on fsck to fsckd communication Socket.
systemd[1]: Reached target Encrypted Volumes.
[ OK ] Reached target Encrypted Volumes.
systemd[1]: Listening on Journal Socket.
[ OK ] Listening on Journal Socket.
systemd[1]: Starting Load Kernel Modules...
Starting Load Kernel Modules...
systemd[1]: Started Read required files in advance.
[ OK ] Started Read required files in advance.
systemd[1]: Mounting Debug File System...
Mounting Debug File System...
systemd[1]: Starting Nameserver information manager...
Starting Nameserver information manager...
systemd[1]: Starting Create list of required static device nodes for the current kernel...
Starting Create list of required st... nodes for the current kernel...
systemd[1]: Starting Journal Service...
Starting Journal Service...
systemd[1]: Starting Restore / save the current clock...
Starting Restore / save the current clock...
systemd[1]: Starting Set console keymap...
Starting Set console keymap...
systemd[1]: Mounted Debug File System.
[ OK ] Mounted Debug File System.
systemd[1]: systemd-modules-load.service: Main process exited, code=exited, status=1/FAILURE
systemd[1]: Failed to start Load Kernel Modules.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
systemd[1]: systemd-modules-load.service: Unit entered failed state.
systemd[1]: systemd-modules-load.service: Failed with result 'exit-code'.
systemd[1]: ureadahead.service: Main process exited, code=exited, status=5/NOTINSTALLED
systemd[1]: ureadahead.service: Unit entered failed state.
systemd[1]: ureadahead.service: Failed with result 'exit-code'.
systemd[1]: Started Create list of required static device nodes for the current kernel.
[ OK ] Started Create list of required sta...ce nodes for the current kernel.
systemd[1]: Started Restore / save the current clock.
[ OK ] Started Restore / save the current clock.
systemd[1]: Started Set console keymap.
[ OK ] Started Set console keymap.
systemd[1]: Started Nameserver information manager.
[ OK ] Started Nameserver information manager.
systemd[1]: Started Journal Service.
[ OK ] Started Journal Service.
Starting Create Static Device Nodes in /dev...
Mounting FUSE Control File System...
Starting Apply Kernel Variables...
[ OK ] Mounted FUSE Control File System.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Started Apply Kernel Variables.
Starting udev Kernel Device Manager...
[ OK ] Started udev Kernel Device Manager.
Starting Remount Root and Kernel File Systems...
[ OK ] Started Remount Root and Kernel File Systems.
Starting Flush Journal to Persistent Storage...
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems (Pre).
Starting udev Coldplug all Devices...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started udev Coldplug all Devices.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
DBG sensor data is at 7f010188
[ TIME ] Timed out waiting for device dev-sda1.device.
[DEPEND] Dependency failed for File System Check on /dev/sda1.
[DEPEND] Dependency failed for /boot.
[DEPEND] Dependency failed for Local File Systems.
Starting Set console font and keymap...
[ OK ] Stopped target OEM Configuration.
[ OK ] Started Stop ureadahead data collection 45s after completed startup.
[ OK ] Closed CUPS Scheduler.
[ OK ] Stopped End-user configuration after initial OEM installation.
[ OK ] Stopped Save/Restore Sound Card State.
[ OK ] Stopped getty on tty2-tty6 if dbus and logind are not available.
[ OK ] Stopped Permit User Sessions.
Starting Set console scheme...
[ OK ] Closed UUID daemon activation socket.
[ OK ] Closed Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Stopped Daily apt activities.
[ OK ] Closed Unix socket for apport crash forwarding.
[ OK ] Stopped Trigger resolvconf update for networkd DNS.
[ OK ] Stopped Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Stopped Manage Sound Card State (restore and store).
[ OK ] Stopped Network Manager.
[ OK ] Closed D-Bus System Message Bus Socket.
[ OK ] Closed Socket activation for snappy daemon.
[ OK ] Stopped target Basic System.
[ OK ] Stopped target System Initialization.
Starting Tell Plymouth To Write Out Runtime Data...
Starting Create Volatile Files and Directories...
[ OK ] Started Emergency Shell.
[ OK ] Reached target Emergency Mode.
Starting LSB: AppArmor initialization...
[ OK ] Reached target Paths.
[ OK ] Reached target Sockets.
[ OK ] Started Set console font and keymap.
[ OK ] Started Set console scheme.
[ OK ] Started Tell Plymouth To Write Out Runtime Data.
[ OK ] Started Create Volatile Files and Directories.
[ OK ] Started LSB: AppArmor initialization.
[ OK ] Started ifup for eth0.
[ OK ] Reached target Network.
[ OK ] Reached target System Time Synchronized.
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Update UTMP about System Boot/Shutdown.
Welcome to emergency mode! After Give root password for maintenance
(or press Control-D to continue):
sulogin: failed to execute /bin/bash : No such file or directory

#vi /etc/fstab

proc /proc proc defaults 0 0
/dev/mmcblk0p2 / ext4 defaults,noatime 0 1
/dev/sda1 /boot/ vfat defaults 0 2
~
~
~
~
~
"fstab" 3 lines, 198 characters

0 项奖励
回复

10,056 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Erik,

can you send me output of commands 'lsblk' and 'fdisk -l'?

Radim.

0 项奖励
回复

10,056 次查看
erikraynolds
Contributor IV

# fdisk -l
Disk /dev/ram0: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram1: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram2: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram3: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram4: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram5: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram6: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram7: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram8: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram9: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram10: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram11: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram12: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram13: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram14: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/ram15: 64 MiB, 67108864 bytes, 131072 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 4096 bytes
I/O size (minimum/optimal): 4096 bytes / 4096 bytes


Disk /dev/mmcblk2: 29 GiB, 31104958464 bytes, 60751872 sectors
Units: sectors of 1 * 512 = 512 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disklabel type: dos
Disk identifier: 0xd258a04d

Device Boot Start End Sectors Size Id Type
/dev/mmcblk2p1 2048 2099199 2097152 1G b W95 FAT32
/dev/mmcblk2p2 2099200 60751871 58652672 28G 83 Linux
#

# lsblk
NAME MAJ:MIN RM SIZE RO TYPE MOUNTPOINT
mmcblk2 179:0 0 29G 0 disk
tqmmcblk2p1 179:1 0 1G 0 part
mqmmcblk2p2 179:2 0 28G 0 part /
#

0 项奖励
回复

10,056 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Erik,

return back in the /etc/fstab device /dev/mmcblk2p1 and reboot. Look if the folder /boot is empty. If it is empty run command 'mount -a' and look there again. If there will be some files, the fstab is working, but is there some other problem at boot. You can also try to change the name /dev/mmcblk2p1 by the disk UUID (for example UUID=DA05-A20E). The UUID you can find from command 'blkid'.

Radim.

.

0 项奖励
回复

10,056 次查看
erikraynolds
Contributor IV

As you said '/boot' is empty and after 'mount -a' - there is 'imx6qp-sabreauto.dtb  zImage'.

10,056 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Erik,

there is problem in configuration of kernel. If you want to fix this issue, than recompile the kernel and in the menuconfig check the option "File system ---> Overlay filesystem support".

Radim.

10,056 次查看
erikraynolds
Contributor IV

Hi Radim,

I run it as you suggested:

  • recompile the kernel and in the menuconfig check the option "File system ---> Overlay filesystem support".
  • after I have still in emergency mode
  • modify /etc/fstab 
    proc /proc proc defaults 0 0
    /dev/mmcblk2p2 / ext4 defaults,noatime 0 1
    #/dev/mmcblk2p1 /boot/ vfat defaults 0 2
  • reboot & after installtion process of Ubuntu strated
  • Now running Ubuntu with automatic login + lxde gui !!!
0 项奖励
回复

10,056 次查看
erikraynolds
Contributor IV

boot log:

still some issue 

ubuntu@imx6qp:/etc$ dmesg
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.1.15 (r59400@Latitude) (gcc version 4.8.5 (Linaro GCC 4.8-2015.06) ) #1 SMP PREEMPT Tue Nov 15 12:24:15 CET 2016
[ 0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c53c7d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine model: Freescale i.MX6 Quad Plus SABRE Automotive Board
[ 0.000000] Reserved memory: created CMA memory pool at 0x6a000000, size 320 MiB
[ 0.000000] Reserved memory: initialized node linux,cma, compatible id shared-dma-pool
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] On node 0 totalpages: 524288
[ 0.000000] free_area_init_node: node 0, pgdat 80bcda80, node_mem_map ee757000
[ 0.000000] Normal zone: 3568 pages used for memmap
[ 0.000000] Normal zone: 0 pages reserved
[ 0.000000] Normal zone: 456704 pages, LIFO batch:31
[ 0.000000] HighMem zone: 67584 pages, LIFO batch:15
[ 0.000000] PERCPU: Embedded 12 pages/cpu @ee6fe000 s16960 r8192 d24000 u49152
[ 0.000000] pcpu-alloc: s16960 r8192 d24000 u49152 alloc=12*4096
[ 0.000000] pcpu-alloc: [0] 0 [0] 1 [0] 2 [0] 3
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 520720
[ 0.000000] Kernel command line: console=tty0,115200 root=/dev/mmcblk2p2 rootwait rw video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes)
[ 0.000000] Inode-cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Memory: 1737928K/2097152K available (8295K kernel code, 435K rwdata, 2892K rodata, 432K init, 450K bss, 31544K reserved, 327680K cma-reserved, 270336K highmem)
[ 0.000000] Virtual kernel memory layout:
vector : 0xffff0000 - 0xffff1000 ( 4 kB)
fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
vmalloc : 0xf0000000 - 0xff000000 ( 240 MB)
lowmem : 0x80000000 - 0xef800000 (1784 MB)
pkmap : 0x7fe00000 - 0x80000000 ( 2 MB)
modules : 0x7f000000 - 0x7fe00000 ( 14 MB)
.text : 0x80008000 - 0x80af51c8 (11189 kB)
.init : 0x80af6000 - 0x80b62000 ( 432 kB)
.data : 0x80b62000 - 0x80bcec40 ( 436 kB)
.bss : 0x80bd1000 - 0x80c41a5c ( 451 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Additional per-CPU info printed with stalls.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] L2C-310 erratum 769419 enabled
[ 0.000000] L2C-310 enabling early BRESP for Cortex-A9
[ 0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[ 0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[ 0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[ 0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[ 0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76470001
[ 0.000000] mxc_clocksource_init 3000000
[ 0.000000] Switching to timer-based delay loop, resolution 333ns
[ 0.000007] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[ 0.000022] clocksource mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[ 0.001227] Console: colour dummy device 80x30
[ 0.001665] console [tty0] enabled
[ 0.001692] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[ 0.001734] pid_max: default: 32768 minimum: 301
[ 0.001856] Mount-cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.001886] Mountpoint-cache hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.002533] CPU: Testing write buffer coherency: ok
[ 0.002853] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.002962] Setting up static identity map for 0x10008280 - 0x100082d8
[ 0.060190] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080197] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[ 0.100184] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[ 0.100249] Brought up 4 CPUs
[ 0.100323] SMP: Total of 4 processors activated (24.00 BogoMIPS).
[ 0.100344] CPU: All CPU(s) started in SVC mode.
[ 0.100867] devtmpfs: initialized
[ 0.112467] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[ 0.112872] clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.129226] pinctrl core: initialized pinctrl subsystem
[ 0.130397] NET: Registered protocol family 16
[ 0.139331] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.169668] cpuidle: using governor ladder
[ 0.199661] cpuidle: using governor menu
[ 0.199821] CPU identified as i.MX6QP, silicon rev 1.0
[ 0.226748] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[ 0.226786] hw-breakpoint: maximum watchpoint size is 4 bytes.
[ 0.227746] imx6q-pinctrl 20e0000.iomuxc: no groups defined in /soc/aips-bus@02000000/iomuxc@020e0000/hdmicecgrp
[ 0.228136] imx6q-pinctrl 20e0000.iomuxc: initialized IMX pinctrl driver
[ 0.230855] imx-gpc 20dc000.gpc: no fsl,ldo-bypass found!
[ 0.272408] mxs-dma 110000.dma-apbh: initialized
[ 0.276666] SCSI subsystem initialized
[ 0.276879] libata version 3.00 loaded.
[ 0.277190] usbcore: registered new interface driver usbfs
[ 0.277295] usbcore: registered new interface driver hub
[ 0.277400] usbcore: registered new device driver usb
[ 0.277601] 2000000.aips-bus:usbphy_nop1 supply vcc not found, using dummy regulator
[ 0.277759] 2000000.aips-bus:usbphy_nop2 supply vcc not found, using dummy regulator
[ 0.279947] i2c i2c-1: IMX I2C adapter registered
[ 0.279984] i2c i2c-1: can't use DMA
[ 0.286398] i2c i2c-2: IMX I2C adapter registered
[ 0.286434] i2c i2c-2: can't use DMA
[ 0.286621] Linux video capture interface: v2.00
[ 0.286723] pps_core: LinuxPPS API ver. 1 registered
[ 0.286746] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.286807] PTP clock support registered
[ 0.299711] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.319707] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[ 0.320652] imx-prg 21cc000.prg: driver probed
[ 0.320774] imx-prg 21cd000.prg: driver probed
[ 0.321262] imx-pre 21c8000.pre: driver probed
[ 0.321478] imx-pre 21c9000.pre: driver probed
[ 0.321682] imx-pre 21ca000.pre: driver probed
[ 0.321892] imx-pre 21cb000.pre: driver probed
[ 0.322276] MIPI CSI2 driver module loaded
[ 0.322563] Advanced Linux Sound Architecture Driver Initialized.
[ 0.323729] Bluetooth: Core ver 2.20
[ 0.323791] NET: Registered protocol family 31
[ 0.323814] Bluetooth: HCI device and connection manager initialized
[ 0.323844] Bluetooth: HCI socket layer initialized
[ 0.323871] Bluetooth: L2CAP socket layer initialized
[ 0.323927] Bluetooth: SCO socket layer initialized
[ 0.324862] Switched to clocksource mxc_timer1
[ 0.336097] NET: Registered protocol family 2
[ 0.336781] TCP established hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.336961] TCP bind hash table entries: 16384 (order: 5, 131072 bytes)
[ 0.337238] TCP: Hash tables configured (established 16384 bind 16384)
[ 0.337399] UDP hash table entries: 1024 (order: 3, 32768 bytes)
[ 0.337482] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes)
[ 0.337747] NET: Registered protocol family 1
[ 0.338112] RPC: Registered named UNIX socket transport module.
[ 0.338142] RPC: Registered udp transport module.
[ 0.338160] RPC: Registered tcp transport module.
[ 0.338177] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.338769] CPU PMU: Failed to parse /soc/pmu/interrupt-affinity[0]
[ 0.338840] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[ 0.340185] imx rpmsg driver is registered.
[ 0.341250] Bus freq driver module loaded
[ 0.342427] futex hash table entries: 1024 (order: 4, 65536 bytes)
[ 0.349184] VFS: Disk quotas dquot_6.6.0
[ 0.349401] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.351506] NFS: Registering the id_resolver key type
[ 0.351573] Key type id_resolver registered
[ 0.351593] Key type id_legacy registered
[ 0.351701] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[ 0.352420] fuse init (API version 7.23)
[ 0.356713] bounce: pool size: 64 pages
[ 0.356752] io scheduler noop registered
[ 0.356776] io scheduler deadline registered
[ 0.356959] io scheduler cfq registered (default)
[ 0.359193] backlight supply power not found, using dummy regulator
[ 0.360823] MIPI DSI driver module loaded
[ 0.361086] MIPI DSI driver module loaded
[ 0.363372] mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
[ 0.363428] fbcvt: 1920x1080@60: CVT Name - 2.073M9
[ 0.363560] mxc_sdc_fb fb@0: registered mxc display driver hdmi
[ 0.394986] imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[ 0.468568] Console: switching to colour frame buffer device 240x67
[ 0.491548] mxc_hdmi 20e0000.hdmi_video: Error only one HDMI output support now!
[ 0.491670] mxc_sdc_fb fb@1: NO mxc display driver found!
[ 0.491814] mxc_sdc_fb fb@2: NO mxc display driver found!
[ 0.491955] mxc_sdc_fb fb@3: registered mxc display driver ldb
[ 0.505105] mxc_hdmi 20e0000.hdmi_video: Read EDID again
[ 0.506183] imx-sdma 20ec000.sdma: no iram assigned, using external mem
[ 0.506739] imx-sdma 20ec000.sdma: no event needs to be remapped
[ 0.507237] imx-sdma 20ec000.sdma: loaded firmware 3.3
[ 0.510114] imx-sdma 20ec000.sdma: initialized
[ 0.511947] pfuze100-regulator 1-0008: Full layer: 2, Metal layer: 1
[ 0.512652] pfuze100-regulator 1-0008: FAB: 0, FIN: 0
[ 0.512733] pfuze100-regulator 1-0008: pfuze100 found.
[ 0.530190] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 298, base_baud = 5000000) is a IMX
[ 0.530900] 21f0000.serial: ttymxc3 at MMIO 0x21f0000 (irq = 299, base_baud = 5000000) is a IMX
[ 0.533276] imx sema4 driver is registered.
[ 0.533404] [drm] Initialized drm 1.1.0 20060810
[ 0.533990] [drm] Initialized vivante 1.0.0 20120216 on minor 0
[ 0.543715] brd: module loaded
[ 0.549788] loop: module loaded
[ 0.550343] si476x-core 1-0063: Using default platform data.
[ 0.550709] si476x-core 1-0063: No IRQ number specified, will use polling
[ 0.551046] si476x-core 1-0063: Error while sending command 0x11
[ 0.551142] si476x-core 1-0063: The device in inconsistent power state
[ 0.552618] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
[ 0.552752] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
[ 0.552878] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
[ 0.553004] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
[ 0.555550] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
[ 0.555688] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[ 0.555828] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst
[ 0.557423] scsi host0: ahci-imx
[ 0.557792] ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 313
[ 0.566216] CAN device driver interface
[ 0.572800] 2188000.ethernet supply phy not found, using dummy regulator
[ 0.577599] pps pps0: new PPS source ptp0
[ 0.587127] libphy: fec_enet_mii_bus: probed
[ 0.592040] fec 2188000.ethernet eth0: registered PHC device 0
[ 0.597336] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 0.601658] ehci-mxc: Freescale On-Chip EHCI Host driver
[ 0.606132] usbcore: registered new interface driver usb-storage
[ 0.610439] usbcore: registered new interface driver usb_ehset_test
[ 0.616011] 2184800.usbmisc supply vbus-wakeup not found, using dummy regulator
[ 0.621265] imx_usb 2184000.usb: Can't register ci_hdrc platform device, err=-517
[ 0.625766] imx_usb 2184200.usb: Can't register ci_hdrc platform device, err=-517
[ 0.630524] mousedev: PS/2 mouse device common for all mice
[ 0.635725] egalax_ts 1-0004: Failed to read firmware version
[ 0.639943] egalax_ts: probe of 1-0004 failed with error -5
[ 0.645117] 2-0044 supply vdd not found, using dummy regulator
[ 0.658892] input: isl29023 light sensor as /devices/virtual/input/input1
[ 0.663536] isl29023 2-0044: driver version 1.0 enabled
[ 0.668753] snvs_rtc 20cc000.snvs:snvs-rtc-lp: rtc core: registered 20cc000.snvs:snvs-r as rtc0
[ 0.673291] i2c /dev entries driver
[ 0.678784] IR NEC protocol handler initialized
[ 0.683209] IR RC5(x/sz) protocol handler initialized
[ 0.687624] IR RC6 protocol handler initialized
[ 0.691984] IR JVC protocol handler initialized
[ 0.696369] IR Sony protocol handler initialized
[ 0.700695] IR SANYO protocol handler initialized
[ 0.704987] IR Sharp protocol handler initialized
[ 0.709199] IR MCE Keyboard/mouse protocol handler initialized
[ 0.713390] IR XMP protocol handler initialized
[ 0.717767] mxc_hdmi 20e0000.hdmi_video: create default modelist
[ 0.723349] mxc_v4l2_output v4l2_out: V4L2 device registered as video16
[ 0.723540] mxc_v4l2_output v4l2_out: V4L2 device registered as video17
[ 0.723709] mxc_v4l2_output v4l2_out: V4L2 device registered as video18
[ 0.723878] mxc_v4l2_output v4l2_out: V4L2 device registered as video19
[ 0.725008] 2-000e supply vdd not found, using dummy regulator
[ 0.725060] 2-000e supply vddio not found, using dummy regulator
[ 0.725101] mag3110 2-000e: check mag3110 chip ID
[ 0.726058] input: mag3110 as /devices/virtual/input/input2
[ 0.727881] mag3110 2-000e: mag3110 is probed
[ 0.728041] 2-001c supply vdd not found, using dummy regulator
[ 0.728107] 2-001c supply vddio not found, using dummy regulator
[ 0.849268] input: mma845x as /devices/virtual/input/input3
[ 0.850673] imx2-wdt 20bc000.wdog: timeout 60 sec (nowayout=0)
[ 0.850864] Bluetooth: HCI UART driver ver 2.3
[ 0.850869] Bluetooth: HCI UART protocol H4 registered
[ 0.850873] Bluetooth: HCI UART protocol BCSP registered
[ 0.850876] Bluetooth: HCI UART protocol ATH3K registered
[ 0.850971] usbcore: registered new interface driver bcm203x
[ 0.851047] usbcore: registered new interface driver btusb
[ 0.851119] usbcore: registered new interface driver ath3k
[ 0.851593] sdhci: Secure Digital Host Controller Interface driver
[ 0.851596] sdhci: Copyright(c) Pierre Ossman
[ 0.851606] sdhci-pltfm: SDHCI platform and OF driver helper
[ 0.852441] /soc/aips-bus@02100000/usdhc@02190000: voltage-ranges unspecified
[ 0.852469] sdhci-esdhc-imx 2190000.usdhc: Got CD GPIO
[ 0.853890] sdhci-esdhc-imx 2190000.usdhc: No vmmc regulator found
[ 0.853896] sdhci-esdhc-imx 2190000.usdhc: No vqmmc regulator found
[ 0.908328] mmc0: SDHCI controller on 2190000.usdhc [2190000.usdhc] using ADMA
[ 0.909470] /soc/aips-bus@02100000/usdhc@02198000: voltage-ranges unspecified
[ 0.909497] sdhci-esdhc-imx 2198000.usdhc: Got CD GPIO
[ 0.909512] sdhci-esdhc-imx 2198000.usdhc: Got WP GPIO
[ 0.909933] sdhci-esdhc-imx 2198000.usdhc: No vqmmc regulator found
[ 0.914914] ata1: SATA link down (SStatus 0 SControl 300)
[ 0.914956] ahci-imx 2200000.sata: no device found, disabling link.
[ 0.914962] ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
[ 0.956066] mmc2: SDHCI controller on 2198000.usdhc [2198000.usdhc] using ADMA
[ 0.957431] 218c000.mlb supply reg_nvcc not found, using dummy regulator
[ 0.957482] mxc_mlb150 218c000.mlb: enalbe regulator
[ 0.958691] mxc_vpu 2040000.vpu_fsl: VPU initialized
[ 0.959265] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[ 0.959484] imx6q-pinctrl 20e0000.iomuxc: unable to find group for node hdmicecgrp
[ 0.959752] imx6q-pinctrl 20e0000.iomuxc: unable to find group for node hdmicecgrp
[ 0.959761] mxc_hdmi_cec soc:hdmi_cec@00120000: can't get/select CEC pinctrl
[ 0.960772] Galcore version 5.0.11.41671
[ 1.261610] mmc2: new ultra high speed SDR104 SDHC card at address 0007
[ 1.262437] mmcblk2: mmc2:0007 SD32G 28.9 GiB
[ 1.264010] mmcblk2: p1 p2
[ 1.626261] caam 2100000.caam: Entropy delay = 3200
[ 1.687129] caam 2100000.caam: Instantiated RNG4 SH0
[ 1.747889] caam 2100000.caam: Instantiated RNG4 SH1
[ 1.747969] caam 2100000.caam: device ID = 0x0a16010000000000 (Era -524)
[ 1.748072] caam 2100000.caam: job rings = 2, qi = 0
[ 1.820804] caam algorithms registered in /proc/crypto
[ 1.824981] caam_jr 2101000.jr0: registering rng-caam
[ 1.825844] platform caam_sm: blkkey_ex: 4 keystore units available
[ 1.826131] platform caam_sm: 64-bit clear key:
[ 1.826203] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 1.826288] platform caam_sm: 64-bit black key:
[ 1.826355] platform caam_sm: [0000] c3 6a 45 11 83 dd 9e d4
[ 1.826439] platform caam_sm: [0008] a8 15 80 12 45 f6 4d a5
[ 1.826521] platform caam_sm: 128-bit clear key:
[ 1.826589] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 1.826673] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 1.826756] platform caam_sm: 128-bit black key:
[ 1.826824] platform caam_sm: [0000] 73 2d f6 29 b6 f5 e4 e8
[ 1.826909] platform caam_sm: [0008] 26 67 33 b5 ef b8 51 6c
[ 1.826990] platform caam_sm: 192-bit clear key:
[ 1.827058] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 1.827141] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 1.827226] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[ 1.827307] platform caam_sm: 192-bit black key:
[ 1.827375] platform caam_sm: [0000] e4 16 e1 27 b6 71 f8 97
[ 1.827459] platform caam_sm: [0008] 14 91 66 7a 58 b3 b5 bb
[ 1.827544] platform caam_sm: [0016] cb 74 16 ce 7e 76 47 55
[ 1.827629] platform caam_sm: [0024] d1 53 f4 ae b2 97 12 6c
[ 1.827710] platform caam_sm: 256-bit clear key:
[ 1.827777] platform caam_sm: [0000] 00 01 02 03 04 0f 06 07
[ 1.827861] platform caam_sm: [0008] 08 09 0a 0b 0c 0d 0e 0f
[ 1.827946] platform caam_sm: [0016] 10 11 12 13 14 15 16 17
[ 1.828030] platform caam_sm: [0024] 18 19 1a 1b 1c 1d 1e 1f
[ 1.828111] platform caam_sm: 256-bit black key:
[ 1.828180] platform caam_sm: [0000] 58 87 f0 ed f3 04 dc d8
[ 1.831832] platform caam_sm: [0008] 43 9f 10 58 07 23 3d ba
[ 1.835503] platform caam_sm: [0016] fb bd 95 e8 32 b1 05 05
[ 1.839114] platform caam_sm: [0024] e6 ba ba fa af b4 de 49
[ 1.842735] platform caam_sm: 64-bit unwritten blob:
[ 1.846402] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 1.850025] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 1.853590] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 1.857404] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 1.860858] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 1.864215] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 1.867571] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 1.870882] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 1.874110] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 1.877272] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 1.880339] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 1.883400] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 1.886494] platform caam_sm: 128-bit unwritten blob:
[ 1.889493] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 1.892463] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 1.895406] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 1.898248] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 1.901005] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 1.903690] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 1.906364] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 1.908927] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 1.911396] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 1.913872] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 1.916278] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 1.918591] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 1.920825] platform caam_sm: 196-bit unwritten blob:
[ 1.923018] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 1.925239] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 1.927395] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 1.929524] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 1.931650] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 1.933732] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 1.935786] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 1.937779] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 1.939719] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 1.941589] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 1.943423] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 1.945240] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 1.947004] platform caam_sm: 256-bit unwritten blob:
[ 1.948757] platform caam_sm: [0000] 00 00 00 00 00 00 00 00
[ 1.950534] platform caam_sm: [0008] 00 00 00 00 00 00 00 00
[ 1.952273] platform caam_sm: [0016] 00 00 00 00 00 00 00 00
[ 1.953980] platform caam_sm: [0024] 00 00 00 00 00 00 00 00
[ 1.955691] platform caam_sm: [0032] 00 00 00 00 00 00 00 00
[ 1.957354] platform caam_sm: [0040] 00 00 00 00 00 00 00 00
[ 1.958982] platform caam_sm: [0048] 00 00 00 00 00 00 00 00
[ 1.960579] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 1.962140] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 1.963669] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 1.965200] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 1.966692] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 1.968373] platform caam_sm: 64-bit black key in blob:
[ 1.969828] platform caam_sm: [0000] ab 12 a6 e2 d7 1e 9b 9a
[ 1.971295] platform caam_sm: [0008] c9 de 29 dd 7e 13 30 fe
[ 1.972763] platform caam_sm: [0016] 9f ab ab 29 8d 8b 14 74
[ 1.974224] platform caam_sm: [0024] a3 81 19 c8 06 41 df 88
[ 1.975706] platform caam_sm: [0032] e6 90 f2 c0 82 c8 77 f2
[ 1.977163] platform caam_sm: [0040] c1 ea 9f 78 f7 9e 7a 25
[ 1.978622] platform caam_sm: [0048] 39 6e eb de b9 46 81 d8
[ 1.980076] platform caam_sm: [0056] 00 00 00 00 00 00 00 00
[ 1.981541] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 1.982971] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 1.984367] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 1.985764] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 1.987114] platform caam_sm: 128-bit black key in blob:
[ 1.988472] platform caam_sm: [0000] c3 3d f1 e6 de e2 2e d3
[ 1.989831] platform caam_sm: [0008] 83 23 f3 2a a0 09 34 07
[ 1.991184] platform caam_sm: [0016] 2d 27 52 8f 39 24 92 d1
[ 1.992554] platform caam_sm: [0024] 97 23 cc f3 cf ff af d6
[ 1.993951] platform caam_sm: [0032] 04 6e 90 c6 c0 10 5e 6b
[ 1.995427] platform caam_sm: [0040] 83 3e 91 b4 7b a7 f4 b5
[ 1.996882] platform caam_sm: [0048] 80 fa 4f c6 3e ea 9d 53
[ 1.998353] platform caam_sm: [0056] 70 2d ff fb 90 14 49 c1
[ 1.999854] platform caam_sm: [0064] 00 00 00 00 00 00 00 00
[ 2.001372] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 2.002889] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.004408] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.005950] platform caam_sm: 192-bit black key in blob:
[ 2.007511] platform caam_sm: [0000] 2a 76 44 24 27 11 da d3
[ 2.009069] platform caam_sm: [0008] 18 07 9b 8e b4 73 79 d5
[ 2.010620] platform caam_sm: [0016] 9a 8f 56 6b 69 72 81 38
[ 2.012189] platform caam_sm: [0024] 85 5d ed 88 01 82 4f 54
[ 2.013786] platform caam_sm: [0032] db 8f 84 ea 01 10 50 76
[ 2.015428] platform caam_sm: [0040] ac 6f 42 8a 1d b7 da 48
[ 2.017080] platform caam_sm: [0048] 83 ec 7e da 02 66 1e e2
[ 2.018750] platform caam_sm: [0056] 52 19 c4 98 11 15 c5 94
[ 2.020449] platform caam_sm: [0064] ff f3 0f 33 e7 68 b6 1f
[ 2.022173] platform caam_sm: [0072] 00 00 00 00 00 00 00 00
[ 2.023922] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.025695] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.027447] platform caam_sm: 256-bit black key in blob:
[ 2.029228] platform caam_sm: [0000] 5e c1 d4 4e 78 da aa 0d
[ 2.031012] platform caam_sm: [0008] 8c cd 90 06 69 60 34 69
[ 2.032787] platform caam_sm: [0016] 63 96 87 54 3c 9c 04 ca
[ 2.034588] platform caam_sm: [0024] f9 fe b0 cf 8d 1f c8 cd
[ 2.036433] platform caam_sm: [0032] 47 64 75 0a 87 27 dc d3
[ 2.038294] platform caam_sm: [0040] 4e a8 5d a5 ba 47 e0 ce
[ 2.040171] platform caam_sm: [0048] b5 75 6c fe 47 20 e2 45
[ 2.042070] platform caam_sm: [0056] c0 44 ba 3b 51 77 c3 eb
[ 2.043997] platform caam_sm: [0064] f5 55 bd c5 dc ac 54 55
[ 2.046022] platform caam_sm: [0072] c3 ca c8 bd 3d 46 22 f0
[ 2.048013] platform caam_sm: [0080] 00 00 00 00 00 00 00 00
[ 2.050021] platform caam_sm: [0088] 00 00 00 00 00 00 00 00
[ 2.052237] platform caam_sm: restored 64-bit black key:
[ 2.054282] platform caam_sm: [0000] 1b e4 1c 21 97 f2 32 2e
[ 2.056358] platform caam_sm: [0008] e5 01 29 5d 3b 48 35 8e
[ 2.058398] platform caam_sm: restored 128-bit black key:
[ 2.060456] platform caam_sm: [0000] 73 2d f6 29 b6 f5 e4 e8
[ 2.062556] platform caam_sm: [0008] 26 67 33 b5 ef b8 51 6c
[ 2.064676] platform caam_sm: restored 192-bit black key:
[ 2.066860] platform caam_sm: [0000] e4 16 e1 27 b6 71 f8 97
[ 2.069064] platform caam_sm: [0008] 14 91 66 7a 58 b3 b5 bb
[ 2.071291] platform caam_sm: [0016] 24 2b 8b 99 29 68 c5 04
[ 2.073540] platform caam_sm: [0024] 2a 86 4b ec 0a bb 8c 86
[ 2.075837] platform caam_sm: restored 256-bit black key:
[ 2.078147] platform caam_sm: [0000] 58 87 f0 ed f3 04 dc d8
[ 2.080489] platform caam_sm: [0008] 43 9f 10 58 07 23 3d ba
[ 2.082856] platform caam_sm: [0016] fb bd 95 e8 32 b1 05 05
[ 2.085228] platform caam_sm: [0024] e6 ba ba fa af b4 de 49
[ 2.087875] snvs-secvio 20cc000.caam-snvs: can't get snvs clock
[ 2.090337] snvs-secvio 20cc000.caam-snvs: violation handlers armed - non-secure state
[ 2.093235] usbcore: registered new interface driver usbhid
[ 2.095752] usbhid: USB HID core driver
[ 2.115526] cs42xx8 1-0048: found device, revision 4
[ 2.120498] fsl-asrc 2034000.asrc: driver registered
[ 2.178946] imx-cs42888 sound-cs42888: cs42888 <-> 2024000.esai mapping ok
[ 2.185121] imx-cs42888 sound-cs42888: snd-soc-dummy-dai <-> 2034000.asrc mapping ok
[ 2.187922] imx-cs42888 sound-cs42888: cs42888 <-> 2024000.esai mapping ok
[ 2.195537] imx-spdif sound-spdif: snd-soc-dummy-dai <-> 2004000.spdif mapping ok
[ 2.199759] imx-tuner-si476x sound-fm: failed to find FM platform device
[ 2.202666] imx-tuner-si476x: probe of sound-fm failed with error -22
[ 2.208284] imx-audio-hdmi sound-hdmi: hdmi-hifi <-> soc:hdmi_audio@00120000 mapping ok
[ 2.212074] NET: Registered protocol family 26
[ 2.215953] NET: Registered protocol family 10
[ 2.219951] sit: IPv6 over IPv4 tunneling driver
[ 2.223625] NET: Registered protocol family 17
[ 2.226680] can: controller area network core (rev 20120528 abi 9)
[ 2.229818] NET: Registered protocol family 29
[ 2.232899] can: raw protocol (rev 20120528)
[ 2.236005] can: broadcast manager protocol (rev 20120528 t)
[ 2.239146] can: netlink gateway (rev 20130117) max_hops=1
[ 2.242624] Bluetooth: RFCOMM TTY layer initialized
[ 2.245900] Bluetooth: RFCOMM socket layer initialized
[ 2.249175] Bluetooth: RFCOMM ver 1.11
[ 2.252421] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[ 2.255692] Bluetooth: BNEP filters: protocol multicast
[ 2.258964] Bluetooth: BNEP socket layer initialized
[ 2.262229] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[ 2.265555] Bluetooth: HIDP socket layer initialized
[ 2.268917] 8021q: 802.1Q VLAN Support v1.8
[ 2.272290] Key type dns_resolver registered
[ 2.284802] can-stby: supplied by can-en
[ 2.288295] flexcan 2094000.flexcan: device registered (reg_base=f0648000, irq=31)
[ 2.296428] ci_hdrc ci_hdrc.0: EHCI Host Controller
[ 2.299233] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[ 2.314914] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[ 2.318496] hub 1-0:1.0: USB hub found
[ 2.321393] hub 1-0:1.0: 1 port detected
[ 2.328895] ci_hdrc ci_hdrc.1: EHCI Host Controller
[ 2.331806] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
[ 2.354887] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[ 2.358476] hub 2-0:1.0: USB hub found
[ 2.361444] hub 2-0:1.0: 1 port detected
[ 2.366045] dhd_module_init in
[ 2.370153] input: gpio-keys as /devices/soc0/gpio-keys/input/input4
[ 2.373500] snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 2016-04-21 14:24:32 UTC (1461248672)
[ 2.386767] can-stby: disabling
[ 2.389901] can-en: disabling
[ 2.393002] SW4: disabling
[ 2.398184] ALSA device list:
[ 2.402086] #0: cs42888-audio
[ 2.405976] #1: imx-spdif
[ 2.409835] #2: imx-hdmi-soc
[ 2.420726] kjournald starting. Commit interval 5 seconds
[ 2.456781] EXT3-fs (mmcblk2p2): using internal journal
[ 2.460715] EXT3-fs (mmcblk2p2): mounted filesystem with ordered data mode
[ 2.464700] VFS: Mounted root (ext3 filesystem) on device 179:2.
[ 2.470344] devtmpfs: mounted
[ 2.475059] Freeing unused kernel memory: 432K (80af6000 - 80b62000)
[ 2.634944] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[ 2.748746] random: systemd urandom read with 15 bits of entropy available
[ 2.755764] systemd[1]: systemd 229 running in system mode. (+PAM +AUDIT +SELINUX +IMA +APPARMOR +SMACK +SYSVINIT +UTMP +LIBCRYPTSETUP +GCRYPT +GNUTLS +ACL +XZ -LZ4 +SECCOMP +BLKID +ELFUTILS +KMOD -IDN)
[ 2.760840] systemd[1]: Detected architecture arm.
[ 2.784657] systemd[1]: Set hostname to <imx6qp>.
[ 2.790838] hub 1-1:1.0: USB hub found
[ 2.795746] hub 1-1:1.0: 4 ports detected
[ 3.094930] usb 1-1.2: new low-speed USB device number 3 using ci_hdrc
[ 3.235378] input: PixArt Dell MS116 USB Optical Mouse as /devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb1/1-1/1-1.2/1-1.2:1.0/0003:413C:301A.0001/input/input5
[ 3.240671] hid-generic 0003:413C:301A.0001: input: USB HID v1.11 Mouse [PixArt Dell MS116 USB Optical Mouse] on usb-ci_hdrc.0-1.2/input0
[ 3.284616] systemd[1]: Listening on udev Kernel Socket.
[ 3.295723] systemd[1]: Listening on Syslog Socket.
[ 3.306182] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
[ 3.316777] systemd[1]: Created slice System Slice.
[ 3.327058] systemd[1]: Reached target Encrypted Volumes.
[ 3.337531] systemd[1]: Created slice User and Session Slice.
[ 3.344927] usb 1-1.3: new low-speed USB device number 4 using ci_hdrc
[ 3.353498] systemd[1]: Set up automount Arbitrary Executable File Formats File System Automount Point.
[ 3.364417] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
[ 3.375388] systemd[1]: Reached target User and Group Name Lookups.
[ 3.386530] systemd[1]: Listening on udev Control Socket.
[ 3.397747] systemd[1]: Listening on fsck to fsckd communication Socket.
[ 3.408502] systemd[1]: Reached target Remote File Systems (Pre).
[ 3.417525] systemd[1]: Reached target Remote File Systems.
[ 3.426685] systemd[1]: Reached target Slices.
[ 3.435813] systemd[1]: Listening on Journal Socket.
[ 3.446642] systemd[1]: Mounting Debug File System...
[ 3.466467] input: DELL Dell USB Entry Keyboard as /devices/soc0/soc/2100000.aips-bus/2184000.usb/ci_hdrc.0/usb1/1-1/1-1.3/1-1.3:1.0/0003:413C:2107.0002/input/input6
[ 3.467486] systemd[1]: Starting Load Kernel Modules...
[ 3.484992] systemd[1]: Starting Set console keymap...
[ 3.498424] systemd[1]: Starting Create list of required static device nodes for the current kernel...
[ 3.511119] systemd[1]: Starting Nameserver information manager...
[ 3.535328] hid-generic 0003:413C:2107.0002: input: USB HID v1.11 Keyboard [DELL Dell USB Entry Keyboard] on usb-ci_hdrc.0-1.3/input0
[ 3.541705] systemd[1]: Starting Restore / save the current clock...
[ 3.556733] systemd[1]: Listening on Journal Socket (/dev/log).
[ 3.572898] systemd[1]: Starting Uncomplicated firewall...
[ 3.588047] systemd[1]: Reached target Swap.
[ 3.616716] systemd[1]: Starting Journal Service...
[ 3.633592] systemd[1]: Mounted Debug File System.
[ 3.648819] systemd[1]: systemd-modules-load.service: Main process exited, code=exited, status=1/FAILURE
[ 3.656670] systemd[1]: Failed to start Load Kernel Modules.
[ 3.676519] systemd[1]: systemd-modules-load.service: Unit entered failed state.
[ 3.688794] systemd[1]: systemd-modules-load.service: Failed with result 'exit-code'.
[ 3.696268] systemd[1]: Started Create list of required static device nodes for the current kernel.
[ 3.713811] systemd[1]: Started Restore / save the current clock.
[ 3.735758] systemd[1]: Started Uncomplicated firewall.
[ 3.747473] systemd[1]: Started Set console keymap.
[ 3.760402] systemd[1]: Started Nameserver information manager.
[ 3.922449] systemd[1]: Started Journal Service.
[ 20.977437] systemd-journald[206]: Received request to flush runtime journal from PID 1
[ 21.995493] DBG sensor data is at 7f010188
[ 22.819378] random: nonblocking pool is initialized
[ 22.955717] fec 2188000.ethernet eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=2188000.ethernet:01, irq=-1)
[ 23.005029] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 26.955379] fec 2188000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 26.955404] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 34.028833] FAT-fs (mmcblk2p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.

0 项奖励
回复

10,056 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Erik,

Can you please send me output of "systemctl status systemd-modules-load.service". Do you have connected some touchscreen or fm device to the board?

Radim.

0 项奖励
回复

10,056 次查看
erikraynolds
Contributor IV

ubuntu@imx6qp:~$ systemctl status systemd-modules-load.service
● systemd-modules-load.service - Load Kernel Modules
Loaded: loaded (/lib/systemd/system/systemd-modules-load.service; static; ven
Active: failed (Result: exit-code) since Thru 2016-02-11 17:28:00 CET; 9 months
Docs: man:systemd-modules-load.service(8)
man:modules-load.d(5)
Process: 193 ExecStart=/lib/systemd/systemd-modules-load (code=exited, status=
Main PID: 193 (code=exited, status=1/FAILURE)
ubuntu@imx6qp:~$

I don't have touchscreen connected just regular HDMI LCD monitor. What you mean "fm" device? 

0 项奖励
回复

10,056 次查看
radimkratochvil
NXP Employee
NXP Employee

I mean some FM radio, or FM transceiver, because this error:

[ 2.199759] imx-tuner-si476x sound-fm: failed to find FM platform device

just saying, that the kernel did not find any FM device.

This error is the same as the one above, but is about touchsreen device:

[ 0.635725] egalax_ts 1-0004: Failed to read firmware version

Please try to run this binary "/lib/systemd/systemd-modules-load" and send me the output. Send me also output from command "journalctl _PID=193" (you can find the PID in the command "systemctl status systemd-modules-load.service")

Radim.

0 项奖励
回复

10,056 次查看
erikraynolds
Contributor IV

run this binary "/lib/systemd/systemd-modules-load" and send me the output

ubuntu@imx6qp:/lib/systemd$ sudo ./systemd-modules-load
[sudo] password for ubuntu:
Failed to find module 'lp'
Failed to find module 'ppdev'
Failed to find module 'parport_pc'
Failed to find module 'snd_bcm2835'
Failed to find module 'bcm2708_rng'

output from command "journalctl _PID=193"

ubuntu@imx6qp:/$ sudo journalctl _PID=193
-- No entries --
ubuntu@imx6qp:/$

actual PID:

output from command "journalctl _PID=187"

ubuntu@imx6qp:/$ systemctl status systemd-modules-load.service
● systemd-modules-load.service - Load Kernel Modules
Loaded: loaded (/lib/systemd/system/systemd-modules-load.service; static; ven
Active: failed (Result: exit-code) since Po 2016-11-21 23:17:01 CET; 4min 50s
Docs: man:systemd-modules-load.service(8)
man:modules-load.d(5)
Process: 187 ExecStart=/lib/systemd/systemd-modules-load (code=exited, status=
Main PID: 187 (code=exited, status=1/FAILURE)
ubuntu@imx6qp:/$
ubuntu@imx6qp:/$ sudo journalctl _PID=187
-- Logs begin at Po 2016-11-21 23:17:01 CET, end at Po 2016-11-21 23:22:25 CET. --
lis 21 23:17:01 imx6qp systemd-modules-load[187]: Failed to find module 'lp'
lis 21 23:17:01 imx6qp systemd-modules-load[187]: Failed to find module 'ppdev'
lis 21 23:17:01 imx6qp systemd-modules-load[187]: Failed to find module 'parport_pc'
lis 21 23:17:01 imx6qp systemd-modules-load[187]: Failed to find module 'snd_bcm2835'
lis 21 23:17:01 imx6qp systemd-modules-load[187]: Failed to find module 'bcm2708_rng'
ubuntu@imx6qp:/$

0 项奖励
回复

10,056 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Erik,

in the file "/etc/modules-load.d/cups-filters.conf " comment out lines with lp, ppdev, parport_pc. Can you send me content of yours folders "/etc/modules-load.d/", "/run/modules-load.d/" and "/usr/lib/modules-load.d/"?

Radim.

0 项奖励
回复

10,056 次查看
erikraynolds
Contributor IV

ubuntu@imx6qp:/etc/modules-load.d$ ls -all
total 24
drwxr-xr-x 2 root root 4096 dub 21 2016 .
drwxr-xr-x 130 root root 12288 lis 21 18:24 ..
-rw-r--r-- 1 root root 119 lis 15 13:04 cups-filters.conf
lrwxrwxrwx 1 root root 10 říj 26 15:26 modules.conf -> ../modules
-rw-r--r-- 1 root root 24 lis 15 13:04 rpi2.conf
ubuntu@imx6qp:/etc/modules-load.d$

ubuntu@imx6qp:/usr/lib/modules-load.d$ ls -all
total 24
drwxr-xr-x 2 root root 4096 lis 15 13:07 .
drwxr-xr-x 110 root root 20480 lis 21 18:40 ..
ubuntu@imx6qp:/usr/lib/modules-load.d$

at /run there is none "/run/modules-load.d/" directory

ubuntu@imx6qp:/run$ ls
agetty.reload initctl mount shm udisks2
alsa irqbalance.pid network snapd.socket user
avahi-daemon lightdm NetworkManager sshd utmp
crond.pid lightdm.pid ntpd.pid sshd.pid uuidd
crond.reboot lock resolvconf sudo
cups log rngd.pid systemd
dbus mlocate.daily.lock rsyslogd.pid tmpfiles.d
dhclient.eth0.pid motd.dynamic sendsigs.omit.d udev
ubuntu@imx6qp:/run$

0 项奖励
回复

10,048 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Erik,

you have to find in this files lines with snd_bcm2835, bcm2708_rng and comment out them. Also look in the file /etc/modules.

Radim.

0 项奖励
回复

10,055 次查看
erikraynolds
Contributor IV

Yes, I did it as suggested but still within "emergency mode"

0 项奖励
回复

10,055 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Erik,

You can use workaround, that you can delete (or comment out) the line in the /etc/stab with the /dev/mmcblk2p1. At least you will not be in the emergency mode and the only think, that you will lost is possibility to edit uboot from the linux (you can always mount it manualy). I was able to reproduce this issue, so I will try to find the problem.

Radim.

10,056 次查看
erikraynolds
Contributor IV

Hi Radim,

here is the log:

# systemctl status systemd-modules-load.service
? systemd-modules-load.service - Load Kernel Modules
Loaded: loaded (/lib/systemd/system/systemd-modules-load.service; static; ven
Active: failed (Result: exit-code) since Thu 2016-02-11 16:28:01 UTC; 2 month
Docs: man:systemd-modules-load.service(8)
man:modules-load.d(5)
Process: 187 ExecStart=/lib/systemd/systemd-modules-load (code=exited, status=
Main PID: 187 (code=exited, status=1/FAILURE)

Warning: Journal has been rotated since unit was started. Log output is incomple

0 项奖励
回复

10,056 次查看
radimkratochvil
NXP Employee
NXP Employee

Hi Erik,

you can disable this module by:

$ sudo systemctl disable ureadahead.service
$ sudo systemctl mask ureadahead.service

This module shouldn't be even install, because it is unnecessary when is there systemd.

0 项奖励
回复