Some GStreamer issues while capturing while preview is active

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Some GStreamer issues while capturing while preview is active

ソリューションへジャンプ
2,986件の閲覧回数
uwekaiser
Contributor I

Hi,

we want to record a mp4 file while preview(overlay) is running.

We have a application which activates the overlay an records a mp4 file on user input.

The error can also be reproduced using gst-launch.  (gst-fsl-plugin-2.0.3)

With the gstreamer pipe

gst-launch mfw_v4lsrc capture-width=640 capture-height=480 num-buffers=150 ! mfw_ipucsc ! 'video/x-raw-yuv,width=640,height=480,framerate=30/1,format=(fourcc)I420' ! queue ! mfw_vpuencoder codec_type=std_mpeg4 qp=5 ! 'video/mpeg,mpegversion=4,framerate=30/1,width=640,height=480' ! mp4mux ! filesink location=test.mp4

I get this output and it works.

MFW_GST_V4LSRC_PLUGIN 2.0.3 build on Jun 7 2012 14:48:18.

IPU_CSC_CORE_LIBRARY_VERSION_INFOR_01.00.

MFW_GST_IPU_CSC_PLUGIN 2.0.3 build on Jun 7 2012 14:47:53.

Setting pipeline to PAUSED ...

[INFO] Product Info: i.MX53

VPU Version: firmware 1.4.48; libvpu: 5.3.2

MFW_GST_VPU_ENCODER_PLUGIN 2.0.3 build on Jun 7 2012 14:47:56.

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

mfw_gst_ipu_csc_get_unit_size:size=614400

mfw_gst_ipu_csc_get_unit_size:size=460800

Got EOS from element ""pipeline0"".

Execution ended after 20664847635 ns.

Setting pipeline to PAUSED ...

Setting pipeline to READY ...

Setting pipeline to NULL ...

Freeing pipeline ...

With preview=true

gst-launch mfw_v4lsrc capture-width=640 capture-height=480 num-buffers=150 preview=true ! mfw_ipucsc ! 'video/x-raw-yuv,width=640,height=480,framerate=30/1,format=(fourcc)I420' ! queue ! mfw_vpuencoder codec_type=std_mpeg4 qp=5 ! 'video/mpeg,mpegversion=4,framerate=30/1,width=640,height=480' ! mp4mux ! filesink location=test.mp4

I get

MFW_GST_V4LSRC_PLUGIN 2.0.3 build on Jun 7 2012 14:48:18.

IPU_CSC_CORE_LIBRARY_VERSION_INFOR_01.00.

MFW_GST_IPU_CSC_PLUGIN 2.0.3 build on Jun 7 2012 14:47:53.

Setting pipeline to PAUSED ...

[INFO] Product Info: i.MX53

VPU Version: firmware 1.4.48; libvpu: 5.3.2

MFW_GST_VPU_ENCODER_PLUGIN 2.0.3 build on Jun 7 2012 14:47:56.

[ 444.360024] mxc_ipu mxc_ipu: IPU Error - IPU_INT_STAT_5 = 0x00200000

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstSystemClock

[ 459.363352] ERROR: v4l2 capture: mxc_v4l_dqueue timeout enc_counter 0

ERROR: from element /GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0: Internal data flow error.

Additional debug info:

gstbasesrc.c(2507): gst_base_src_loop (): /GstPipeline:pipeline0/MFWGstV4LSrc:mfwgstv4lsrc0:

streaming task paused, reason error (-5)

Execution ended after 10001064875 ns.

Setting pipeline to PAUSED ...

Setting pipeline to READY ...

Setting pipeline to NULL ...

Freeing pipeline ...


ラベル(1)
タグ(2)
1 解決策
2,079件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Seems you just added a "preview=true" is not enough.

Please see this link for your reference.

< https://community.freescale.com/message/292568#292568 >


元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,080件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Seems you just added a "preview=true" is not enough.

Please see this link for your reference.

< https://community.freescale.com/message/292568#292568 >


0 件の賞賛
返信