SoloX field upgrade through Ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SoloX field upgrade through Ethernet

1,309件の閲覧回数
ScottKerstein
Contributor III

Hello,

It's desired to get field upgrades via an Ethernet connection through a IOT website connection.  Are there any app notes might exist to doing this on a SoloX, or just i.MX6 in general?

    1. Need a way to ensure a failed upgrade does not compromise the machine and not enable it to take a subsequent upgrade
    2. Would like a way to separate out the images so the GUI application can be upgraded separately from the rootfs and kernel
    3. Would like to be able to sign and possibly encrypt the upgrade images.

Thanks, in advance.

Scott

ラベル(3)
0 件の賞賛
返信
2 返答(返信)

1,162件の閲覧回数
JasonMoss
NXP Employee
NXP Employee

Scott,

You may want to check out work done in the community by Stefano Babic at Denx (i.MX U-boot Custodian).

Updating an embedded system — Embedded Software Update Documentation 2014.07 documentation

Here is a recent presentation on the topic:
http://events.linuxfoundation.org/sites/events/files/slides/SoftwareUpdateForEmbedded.pdf

Jason

317.908.5314

0 件の賞賛
返信

1,162件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

It seems that you want to have something similar to what Google Play does, in Android which allows to upgrade the application without touching the system just the application,  I would recommend to use Android as platform, and customize it, since it is prepared to such application

0 件の賞賛
返信