SoloX RMII ENET1_REF_CLK Jitter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SoloX RMII ENET1_REF_CLK Jitter

1,055 Views
scottgauche
Contributor I


Hi,


Is there a way to determine the jitter specifications of the ENET1_REF_CLK for a RMII interface?

Thanks,

Scott

Labels (2)
0 Kudos
3 Replies

485 Views
art
NXP Employee
NXP Employee

For the RMII interface, the reference clock should be 50MHz +/- 50ppm.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

485 Views
scottgauche
Contributor I

We are using a 24 MHz +/- 30 ppm crystal for the SoloX XTAL.  Similar to what is used on the SoloX Sabre board.  But that is the frequency tolerance, we are looking for a way to figure out if there is a jitter specification for what the SoloX is able to output for the 50 MHz RMII clock to the PHY.

0 Kudos

485 Views
art
NXP Employee
NXP Employee

No, there is no strict jitter specification for this clock. The meaning is that any frequency fluctuation of the clock must remain within this 50MHz +/- 50ppm range.

Artur

0 Kudos