Software Clock Gating on WiFi SDIO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Software Clock Gating on WiFi SDIO

949件の閲覧回数
dhvani-champaneri
Contributor I

We are using the NXP i.MX8MM processor with the 5.15.71 kernel and have ported Murata’s cyw-fmac backported driver(kirkstone Godzilla release) for Murata's Wi-Fi chip module (LBEE5XV2EA). Here, I want to discuss the issue of SDIO clock gating. Specifically, the SDIO clock for the Wi-Fi chip remains enabled continuously even when there is no communication happening over Wi-Fi. I want to enable software clock gating support for the Wi-Fi SDIO interface.

Interestingly, on another SDIO interface where an eMMC is connected, clock gating is already functioning as expected.

Debugging Steps Performed

  1. Driver and Function Analysis:
    • The Murata Wi-Fi brcmfmac driver uses sdio_readl/writel APIs from “mmc/core/sdio_io.c” for read/write operations with the SDIO interface. Which directly reads/writes from the address space of a given SDIO.
    • The i.MX8MM’s SDIO driver (“mmc/host/sdhci-esdhc-imx.c”) performs these operations using readl() which uses IOMEM address with some offset.
  2. Kernel Patch Impact:

There is a specific patch in the kernel where SDIO clock gating support was removed from the SDIO. Here is the commit:

https://patchwork.kernel.org/project/linux-mmc/patch/1443776171-7127-1-git-send-email-ulf.hansson@li...

 

    • I attempted to re-implement clock hold and clock release functionality to gate the clock before every read/write operation from the above commit. However, the Wi-Fi module failed to operate correctly with this implementation.

Attempted Approaches

  1. Clock Gating via mmc_set_ios Operations

       To manage the clock gating, I implemented the following functions in clock_hold and              clock_release:

void mmc_gate_clock(struct mmc_host *host) {

    unsigned long flags;

    spin_lock_irqsave(&host->clk_lock, flags);

    host->clk_old = host->ios.clock;

    host->ios.clock = 0;

    host->clk_gated = true;

    spin_unlock_irqrestore(&host->clk_lock, flags);

    mmc_set_ios(host);

}

 

void mmc_ungate_clock(struct mmc_host *host) {

    if (host->clk_old) {

        BUG_ON(host->ios.clock);

        __mmc_set_clock(host, host->clk_old);

    }

}

  • Description:
    • The mmc_gate_clock() function gates the clock by setting the ios.clock value to 0.
    • The mmc_ungate_clock() function restores the clock using a cached clock value (clk_old).
  • Challenges:
    • These functions rely on ios operations of the host driver.
    • In the i.MX MMC driver (mmc/host/sdhci-esdhc-imx.c), ios operations are not fully implemented. However, there is a mmc_host_ops struct in the driver that allows set_ios partial implementation, which made this approach partially functional.
    • Despite these adjustments, the WiFi module failed to operate correctly.

 

Question:

    • Is there any alternative approach to enable software clock gating on the WiFi SDIO interface?
ラベル(1)
0 件の賞賛
返信
0 返答(返信)