Slow Network on SABRE iMX6Q

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Slow Network on SABRE iMX6Q

ソリューションへジャンプ
2,005件の閲覧回数
constantins
Contributor II

All,

I am having difficulty communicating with my iMX6Q. I am ssh'ed in and symbols appear after some delay. Pinging from the iMX6 to my router, reveals a delay of 100ms! My computer to the iMX6 is 500ms!

  Could anyone offer any debugging advice? Thank you in advance!

Constantin

ラベル(2)
0 件の賞賛
返信
1 解決策
1,599件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try the solution, suggested in


https://community.freescale.com/message/319417#319417

(adding "enable_wait_mode=off" in the bootargs of U-boot)

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
1,600件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please try the solution, suggested in


https://community.freescale.com/message/319417#319417

(adding "enable_wait_mode=off" in the bootargs of U-boot)

0 件の賞賛
返信
1,599件の閲覧回数
constantins
Contributor II

Yuri thank you very much, the difference was instantly visible. Tried booting again without the suggested parameter and the problem re-emerged.

0 件の賞賛
返信
1,599件の閲覧回数
LeonardoSandova
Specialist I

Which BSP version are you using ? L3.0.35_1.1.0? Also, for a more verbose log, add -v to the ssh command

Leo

0 件の賞賛
返信
1,599件の閲覧回数
constantins
Contributor II

Hey Leonardo, I am using the L.3.0.35_1.1.0_121218 uboot binary (u-boot-mx6q-sd.bin) and oneiric file system. I believe I got these from the Downloads sections but I'm having trouble finding them again.

What am I looking for with the ssh -v flag? It seems the entire connection is slow (due to the ping tests?) Thank you

0 件の賞賛
返信
1,599件の閲覧回数
LeonardoSandova
Specialist I

It may be a DNS issue on your side: http://scofaq.aplawrence.com/FAQ_scotec4slow_ping.html

Also, try another filesystem, like the Linux Demo Image; if problem persists, then something is wrong on your network.

0 件の賞賛
返信
1,599件の閲覧回数
constantins
Contributor II

Hey Leonardo, thanks for the link! I tried the ping -n, but experienced the same ping. We have a few other systems running on the network (currently turned off), they do not experience the similar latency's.

My first thought is that this is something I've done in setting up the board (perhaps in uboot?) and is related to a driver setting or maybe version?

0 件の賞賛
返信
1,599件の閲覧回数
LeonardoSandova
Specialist I

I do not think it is U-boot related problem. U-boot is just the loader and you are having issues on the OS.

0 件の賞賛
返信