Single x32 DDR3 Module for i.MX6

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Single x32 DDR3 Module for i.MX6

ソリューションへジャンプ
1,474件の閲覧回数
cayt
Contributor II

Hi,

I am busy sketching a system draft using i.MX6DL with x32bit DDR3 memory. As far as my research goes only the LPDDR3 memories have x32 bit data width but unfortunately i.MX6 devices don't support LPDDR3. The DDR3 and LVDDR3 memories have x16 bit data width only. I know I could use 2 LV/DDR3 modules but space is one of the biggest challenges in the design, that's why I would like to keep it to a single memory module, if possible. Could anyone suggest a direction to go?

Thanks!

ラベル(2)
タグ(4)
0 件の賞賛
返信
1 解決策
1,006件の閲覧回数
cayt
Contributor II

Hi,

By mistake I opened the same discussion twice. Please leave your comments on this discussion

Thanks,

Cahit

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,007件の閲覧回数
cayt
Contributor II

Hi,

By mistake I opened the same discussion twice. Please leave your comments on this discussion

Thanks,

Cahit

0 件の賞賛
返信
1,006件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Cahit

for space constrained designs it may be useful to look at scm modules

http://www.nxp.com/scm

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,006件の閲覧回数
cayt
Contributor II

Hi Igor,

Thanks for the suggestion. I am aware of these chips but the memory technology used is LPDDR2 and I have to use DDR3. BTW, I see that the PMIC MMPF0100 is integrated in the chip. Are there any heat issues with these chips, that you are aware of?

Thanks,

Cahit

0 件の賞賛
返信