Single stepping not working on iMX53 EC7 platform.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Single stepping not working on iMX53 EC7 platform.

跳至解决方案
1,668 次查看
bdp42
Contributor IV

Hi,

I am developing an Embedded Compact 7 based application on an iMX53 platform.

I have generated the SDK for the board and built a simple application using this SDK. I can download the application onto the board and can set breakpoints but single stepping does not work, it simply continues on.

Has anyone seen this kind of problem before or suggest what might be causing this? I am using Visual Studio 2008 with the latest platform builder.

Thanks,

Bruno

标签 (2)
1 解答
1,525 次查看
bdp42
Contributor IV

I discovered the cause of the problem. There is a known issue with Visual Studio 2008 and Embedded Compact 7 and the following update addresses this issue. I have appplied the upadate and single stepping works.

http://support.microsoft.com/kb/2483802

This might be useful to someone else.


在原帖中查看解决方案

2 回复数
1,526 次查看
bdp42
Contributor IV

I discovered the cause of the problem. There is a known issue with Visual Studio 2008 and Embedded Compact 7 and the following update addresses this issue. I have appplied the upadate and single stepping works.

http://support.microsoft.com/kb/2483802

This might be useful to someone else.


1,525 次查看
JerryZeng
NXP Employee
NXP Employee

No, I didn't see such problem.

You'd better contact MSFT on such issue.