Single Channel LVDS to HDMI 1080p30

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Single Channel LVDS to HDMI 1080p30

Jump to solution
978 Views
kirgene
Contributor II

Hello,

I need to know is it possible to transmit 1080p30 signal over single channel LVDS over LVDS-to-HDMI converter (Chrontel CH7036) to get 1080p30 output on HDMI.

I know it's not possible to transmit 1080p30 @ 60Hz with single channel LVDS, but maybe it's possible to transmit 1080p30 @ 30Hz ?

Labels (1)
0 Kudos
1 Solution
604 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yevhen

single channel supports up to WXGA, with IPU data rate up to 85 MHz, as described in p.71

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

so seems 1080p30 may be supported.

Best regards

igor
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
605 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yevhen

single channel supports up to WXGA, with IPU data rate up to 85 MHz, as described in p.71

A Deep Dive into Image Processing for i.MX 6 Series Applications Processors

so seems 1080p30 may be supported.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos