Simple Audio setup in Linux iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simple Audio setup in Linux iMX6

3,774 Views
erezsteinberg
Contributor IV

Hello experts,

I have a simple audio setup on my board. I have an external DAC+Amplifier that connects to iMX6 over I2S and to a speaker (Mono).

There are no controls for the 'codec' -- it just plays what is sent over I2S.

There's no headphone or microphone... just one output with no configuration options.

(iMX6 is I2S Master, for clocking)

Can I use 'simple-audio-card' or something else to easily set up such a configuration?

Regards,

Erez

Labels (2)
Tags (3)
0 Kudos
Reply
1 Reply

2,470 Views
igorpadykov
NXP Employee
NXP Employee

Hi Erez

I am afraid not, just for quick reference please look at attached

documents Chapters Porting Audio Codecs to a Custom Board.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply