Sim Card support in IMX6Q sabre SD board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sim Card support in IMX6Q sabre SD board

598件の閲覧回数
senthilkumar_s1
Contributor II

Hi, all we are developing solution using IMX6Q sabre SD board. It contains one Sim card Slot. But slot is not working while using android Kitkat and lolipop downloaded from free scale site. We need some help regarding how to use that sim slot,even if some extra hardware is required please mention that also.

Thanks in advance.

ラベル(2)
タグ(3)
0 件の賞賛
返信
1 返信

481件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Senthil

that sim slot can be used by usb gsm module (like EM770W)

produced with PCI-e interface.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信