Silicon Revision on iMX8QXP Dev Kit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Silicon Revision on iMX8QXP Dev Kit

2,067 Views
rlumo
Contributor II

I would like to know what is the Silicon Revision on my iMX8QXP Dev Kit.

I have the following stickers on the back of my dev kit:

S/N VV 19420385

SCH-29683 REV C2

700-29683 REV C2

TDA 7239

0 Kudos
Reply
3 Replies

2,015 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,

 

You may try 2 ways to identify the silicon revision for the chip:

 

  • Use "misc_get_control" with "SC_R_SYSTEM" and "SC_C_ID" to get the REV info.
  • Check the last letter of the part number, which indicates the silicon reversion.

 

In your case it may be easier to identify using the second method, simx8qx6avlf1bb -> B0 chip

 

Hope this helps,

Best regards,

Aldo.

0 Kudos
Reply

1,987 Views
darsh_dev
Contributor V
0 Kudos
Reply

2,015 Views
rlumo
Contributor II

Also these are the markings on the chip.

simx8qx6avlf1bb
sbae 1928
1N95W
korea mbaesbc
0 Kudos
Reply