Silex SDCAN module tests

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Silex SDCAN module tests

3,466 Views
seshpadm
Contributor I

Hi,

I'd appreciate if anyone can share basic functionality/performance, WiFi driver performance/memory and other test results for Silex SDCAN module with i.MX6 or any other freescale platform.

Thanks,

SeshPad

Labels (2)
0 Kudos
Reply
3 Replies

3,218 Views
seshpadm
Contributor I

Hi Yuji,

Thank you for providing performance related data w.r.t. data transfer rates. I am trying to assess multiple radio module vendors and we are looking at multiple criteria like power consumption, data rates, handover times, memory footprint, driver execution times etc.. on i.MX6 processor. Any data relevant to these or anything that differentiates Silex from other radio modules will be of great help.

Regards,

SeshPad

0 Kudos
Reply

3,218 Views
YS
Contributor IV

Sesh,

Please contact silex america technical support.

I cannot disclose too much detail here. You may need to sign NDA for more detailed data.

Best Regards,

0 Kudos
Reply

3,218 Views
YS
Contributor IV

This is not an official performance data, neither max possible performance

measured in ideal condition. This is just an example what I saw on my desktop with

iperf (TCP) throughput, in moderately congested radio environment / close

distance (4ft) from consumer-class 802.11n Access Point.

5GHz HT40 transmit 48Mbps

5GHz HT40 receive 52Mbps

2.4GHz HT20 transmit 20Mbps

2.4GHz HT20 receive 25Mbps

Note that you must configure clock governor to "performance" on iMX6 Ubuntu Linux.

echo performance > /sys/devices/system/cpu/cpu0/cpufreq/scaling_governor

echo performance > /sys/devices/system/cpu/cpu1/cpufreq/scaling_governor

echo performance > /sys/devices/system/cpu/cpu2/cpufreq/scaling_governor

echo performance > /sys/devices/system/cpu/cpu3/cpufreq/scaling_governor


The power-on default is "automatic", which significantly reduce CPU performance.

For functionality, do you have specific feature looking for?