Silent reboot after loading Android 9.0.0_p2.3.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Silent reboot after loading Android 9.0.0_p2.3.0

1,293 Views
jeffreymarius
Contributor I

Board Used: IMX8MM EVK DDR4 with CY-43455

Loaded the images using the UUU method and flashed all the images from the following link: https://www.nxp.com/webapp/sps/download/license.jsp?colCode=P9.0.0_2.3.0_ANDROID_SOURCE&appType=file...

UUU command used:
uuu_imx_android_flash.bat -f imx8mm -a -e -d ddr4 -t sd -c 28

Bootargs used:
u-boot=> setenv bootargs console=ttymxc1,115200 earlycon=ec_imx6q,0x30890000,115200 init=/init androidboot.console=ttymxc1 consoleblank=0 androidboot.hardware=freescale cma=800M androidboot.primary_display=imx-drm firmware_class.path=/vendor/firmware transparent_hugepage=never androidboot.wifivendor=bcm androidboot.wificountrycode=CN

u-boot=> setenv append_bootargs androidboot.selinux=permissive

u-boot=> saveenv

u-boot=> boot

After booting the system is rebooting again and again. I am not able to see any suspicious logs or crash. But it is to be noted that when before the board could reboot if I provide "ifconfig wlan0 down" then the board stops rebooting. Not sure if this could be a reason because sometimes reboot is happening even with wlan0 down.

Could you please help me resolve the issue?

Attaching the logs as well.

Tags (2)
0 Kudos
Reply
1 Reply

962 Views
diegoadrian
NXP Employee
NXP Employee

Hello,

Could you please try with the following bootargs?

U-Boot > setenv bootargs console=ttymxc0,115200 earlycon=imxuart,0x30860000,115200
init=/init androidboot.gui_resolution=1080p androidboot.console=ttymxc0 consoleblank=0
androidboot.hardware=freescale cma=1280M androidboot.primary_display=imx-drm
firmware_class.path=/vendor/firmware transparent_hugepage=never
androidboot.fbTileSupport=enable androidboot.wifivendor=qca
androidboot.wificountrycode=CN

U-Boot > setenv append_bootargs androidboot.selinux=permissive
U-Boot > saveenv

Hope this could help you.

Best regards,

Diego.

0 Kudos
Reply