Significance of the different run modes for "VDD_SOC_IN" ? Found for i.MX6UL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Significance of the different run modes for "VDD_SOC_IN" ? Found for i.MX6UL

Jump to solution
895 Views
wowa
Contributor I

Dear Community,

i found some informations in the Datasheet "IMX6ULCEC" under the operating ranges about the input voltages of "VDD_SOC_IN".

Could anyone explain the difference between the Run Modes "LDO enabled", "LDO bypassed" and "Suspend (DSM) Mode" ?

I could not find something in the datasheet or reference manual. And what mode is the standard mode ?

pastedImage_12.png

Thanks beforehand for your efforts.

BR

Wolfgang

Labels (3)
0 Kudos
Reply
1 Solution
757 Views
igorpadykov
NXP Employee
NXP Employee

Hi Walter

Figure 1 i.MX 6UltraLite power rails AN5170 i.MX 6 UltraLite Power Consumption

Measurement shows processor power design. "LDO enabled", standard mode

when core is powered from internal LDO. "LDO bypassed" when LDO is shorted:

VDD_ARM_CAP=VDD_SOC_IN.

DSM is described in sect.4.1.1. Use case 1: Deep-Sleep mode (DSM)

http://cache.freescale.com/files/32bit/doc/app_note/AN5170.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
758 Views
igorpadykov
NXP Employee
NXP Employee

Hi Walter

Figure 1 i.MX 6UltraLite power rails AN5170 i.MX 6 UltraLite Power Consumption

Measurement shows processor power design. "LDO enabled", standard mode

when core is powered from internal LDO. "LDO bypassed" when LDO is shorted:

VDD_ARM_CAP=VDD_SOC_IN.

DSM is described in sect.4.1.1. Use case 1: Deep-Sleep mode (DSM)

http://cache.freescale.com/files/32bit/doc/app_note/AN5170.pdf

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply