Sign Android images with new generated keys.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Sign Android images with new generated keys.

2,756件の閲覧回数
NunoVilaca
Contributor II

We're trying to sign target files with our own keys (generated with the mkkeys.sh script, as described in the FAQ pdf ), but are getting an error:

rewriting BOOT/RAMDISK/default.prop:
replace: ro.bootimage.build.fingerprint=Android/var_mx6/var_mx6:8.0.0/1.0.0-ga/2020072402:user/dev-keys
with: ro.bootimage.build.fingerprint=Android/var_mx6/var_mx6:8.0.0/1.0.0-ga/2020072402:user/release-keys
rewriting RECOVERY/RAMDISK/default.prop:
rewriting RECOVERY/RAMDISK/prop.default:
replace: ro.bootimage.build.fingerprint=Android/var_mx6/var_mx6:8.0.0/1.0.0-ga/2020072402:user/dev-keys
with: ro.bootimage.build.fingerprint=Android/var_mx6/var_mx6:8.0.0/1.0.0-ga/2020072402:user/release-keys
replace: ro.build.display.id=1.0.0-ga dev-keys
with: ro.build.display.id=1.0.0-ga
replace: ro.build.tags=dev-keys
with: ro.build.tags=release-keys
replace: ro.build.description=var_mx6-user 8.0.0 1.0.0-ga 2020072402 dev-keys
with: ro.build.description=var_mx6-user 8.0.0 1.0.0-ga 2020072402 release-keys
replace: ro.build.fingerprint=Android/var_mx6/var_mx6:8.0.0/1.0.0-ga/2020072402:user/dev-keys
with: ro.build.fingerprint=Android/var_mx6/var_mx6:8.0.0/1.0.0-ga/2020072402:user/release-keys
signing: BasicDreams.apk (/home/nvilaca/.android-certs//platform)
java.security.NoSuchAlgorithmException: 1.2.840.113549.1.5.13 SecretKeyFactory not available
at java.base/javax.crypto.SecretKeyFactory.<init>(SecretKeyFactory.java:122)
at java.base/javax.crypto.SecretKeyFactory.getInstance(SecretKeyFactory.java:168)
at com.android.signapk.SignApk.decryptPrivateKey(SignApk.java:238)
at com.android.signapk.SignApk.readPrivateKey(SignApk.java:261)
at com.android.signapk.SignApk.main(SignApk.java:1024)

ERROR: signapk.jar failed: return code 1

Is it the way the keys are generated? Or something missing?

Ubuntu 18.04.1

OpenSSL 1.1.1  11 Sep 2018

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

2,682件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Which MPU are you running it at? -Anyway, the purpose of this is to sign OTA packages, for that, you will need to use the mkkey.sh script for generating the keys, but please remember that it will be required to be run 4 times (for each key) specifying the key name and password for each. The detailed description is addressed in chapter 29 of the following document: https://www.nxp.com/docs/en/reference-manual/Android_Frequently_Asked_Questions.pdf 

Hope that helps!

BR,

Ivan.

0 件の賞賛
返信