Sierra 3G modem in Linux 3.14.28

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Sierra 3G modem in Linux 3.14.28

2,328 Views
fang
Contributor I

Sierra MC8705 modem works fine in Linux 3.10.53 (Sierra_net.c V3.2)

Using this modem on our board(imx6Q SabreSD board), it works in the field for over one year.

Last week I upgraded Linux to 3.14.28(imx_3.14.28_1.0.0_ga) (Sierra_net.c V3.2).

After that, modem is detected but it doesn't work.

    # ifconfig wwan0

    ifconfig: wwan0: error fetching interface information: Device not found

    # dmesg | grep -e sierra -e Sierra

    [    5.009833] usbcore: registered new interface driver sierra

    [    5.016359] usbserial: USB Serial support registered for Sierra USB modem

    [    5.025902] sierra 1-1.2:1.0: Sierra USB modem converter detected

    [    5.068022] usb 1-1.2: Sierra USB modem converter now attached to ttyUSB0

    [    5.076418] sierra 1-1.2:1.1: Sierra USB modem converter detected

    [    5.085750] usb 1-1.2: Sierra USB modem converter now attached to ttyUSB1

    [    5.095794] sierra 1-1.2:1.2: Sierra USB modem converter detected

    [    5.107202] usb 1-1.2: Sierra USB modem converter now attached to ttyUSB2

    [    5.121224] sierra 1-1.2:1.3: Sierra USB modem converter detected

    [    5.132774] usb 1-1.2: Sierra USB modem converter now attached to ttyUSB3

    [    5.143377] sierra 1-1.2:1.4: Sierra USB modem converter detected

    [    5.152881] usb 1-1.2: Sierra USB modem converter now attached to ttyUSB4

    # lsusb

    Bus 001 Device 003: ID 1199:68a3 Sierra Wireless, Inc. MC8700 Modem

    Bus 001 Device 002: ID 0424:2412 Standard Microsystems Corp.

    Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub

    # cat /dev/ttyUSB3

    +CREG: 2,1,"2252","014C0E9E",2

    OK

    *CNTI: 0,UMTS

    OK

    ...

    # dmesg | grep -e pci -e PCI

    [    0.235767] PCI: CLS 0 bytes, default 64

    [    1.403808] imx6q-pcie 1ffc000.pcie: phy link never came up

    [    1.403827] imx6q-pcie 1ffc000.pcie: Failed to bring link up!

    [    1.403858] imx6q-pcie 1ffc000.pcie: failed to initialize host

    [    1.403908] imx6q-pcie: probe of 1ffc000.pcie failed with error -22

    [    2.690746] ehci-pci: EHCI PCI platform driver

    I use the same SIM card, board, modem and rootfs as I tested on Linux 3.10.53.

    Yesterday I read many threads related to modem in this community, and tried below:

    1. Add more delay in imx6_pcie_wait_for_link in pci-imx6.c:

        change to usleep_range(100, 1000), or chang count = 10000

    2. Disable CONFIG_PCI_MSI

    3. Remove #address_cells; #size_cells of intc in imx6qdl.dtsi

    it still no wwan0 interface.

    I'm really appreciate if someone can give me some idea.

    PS. Is there any official released patches for Linux imx_3.14.28_1.0.0_ga?

    Thanks.

Labels (2)
0 Kudos
Reply
1 Reply

1,467 Views
igorpadykov
NXP Employee
NXP Employee

Hi jifang

for 3.14.28 one can look at solutions in

IMX6Q: Linux boot halts at PCIe config space read

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply