Should I use ubuntu 32bit or 64 bit to cross compiler imx7d?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Should I use ubuntu 32bit or 64 bit to cross compiler imx7d?

989 Views
emintolgasivri
Contributor II

My pc has ubuntu 64 bit.Should I use it for imx7d?otherwise Do I have to use ubuntu 32 bit?

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

889 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi Emin,

It is recommended building Yocto for i.MX 6/7/8 using a 64-bit host machine.

For additional Host setup, you could refer to “i.MX Yocto Project User's Guide” document, included on the LINUX_DOCS package, available on this link.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply