Should I use ubuntu 32bit or 64 bit to cross compiler imx7d?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Should I use ubuntu 32bit or 64 bit to cross compiler imx7d?

988件の閲覧回数
emintolgasivri
Contributor II

My pc has ubuntu 64 bit.Should I use it for imx7d?otherwise Do I have to use ubuntu 32 bit?

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

888件の閲覧回数
CarlosCasillas
NXP Employee
NXP Employee

Hi Emin,

It is recommended building Yocto for i.MX 6/7/8 using a 64-bit host machine.

For additional Host setup, you could refer to “i.MX Yocto Project User's Guide” document, included on the LINUX_DOCS package, available on this link.


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信