Short straight lines appear on Qt5 APP (i.MX6Quad SABRE kit)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Short straight lines appear on Qt5 APP (i.MX6Quad SABRE kit)

1,099 Views
coilnpark
Contributor IV

Hi everyone,

I am developing i.MX6 product. When I checked Qt5 APP by using SABRE kit, there was short straight lines.

Could you help me? 

Yocto version : Warrior

Kernel version : L4.19.35

캡처.PNG

0 Kudos
Reply
2 Replies

979 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Coiln,

if issue appears only for 720p and 1080p, this may point to processor

internal buses bandwidth limitation, one can try to decrease fps or change

IPU QoS with i.MX6Q IOMUXC_GPR6, also check About MMDC Profiling Tool for i.MX6 

 Regards

0 Kudos
Reply

979 Views
coilnpark
Contributor IV

Hi Bio,

When I tried 800x480 (7"), 800x600(12"), 1024x768(15"), there was the same issue.

0 Kudos
Reply